Page 10 of 10 FirstFirst ... 678910
Results 91 to 93 of 93

Thread: Trying to debug HROS1 with RPI talking to Arbotix Pro

  1. #91
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    20

    Re: Trying to debug HROS1 with RPI talking to Arbotix Pro

    Quote Originally Posted by LloydF View Post
    Ok, so th RPI-3 Works with the new image from the rpi 2016-02-26 image. Use raspi-config to resize and boot without desktop and https://github.com/Interbotix/HROS1-Framework/wiki for all Debian Dependencies, get clone the framework and everything compiles and runs some 35% Faster (you know i am guessing on the speed increase but it is much faster.) oh yes!! edit note (the wifi built in is really nice and frees up a usb port, so I really dont need a hub. Yea!)(Note still have some Bluetooth issues with the rpi3)
    Hi Lloyd, are you seeing the latency issue with the RPi3?

  2. #92

    Re: Trying to debug HROS1 with RPI talking to Arbotix Pro

    Hi. I have temporarily stopped using the RPi3 until a few more issues are worked out with there image and the new V2.1 camera, but as far as to what does work all you need do is make sure the Desktop is off and unless your running a real time rig like a chopper you should be good.
    Last edited by LloydF; 05-16-2016 at 09:43 PM.

  3. #93
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    20

    Re: Trying to debug HROS1 with RPI talking to Arbotix Pro

    Ok, thanks, sounds good.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. HROS1 Simulator, is Darwin OP similar enough?
    By Johnny in forum HR-OS1 Development and Discussion
    Replies: 2
    Last Post: 07-29-2016, 03:40 AM
  2. HROS1 RPi and ArbotixPro communication
    By az139 in forum Arbotix, Microcontrollers, Arduino
    Replies: 6
    Last Post: 08-24-2015, 01:03 AM
  3. HROS1 - Wifi stopped working?
    By KurtEck in forum Humanoids, Walkers & Crawlers
    Replies: 8
    Last Post: 05-20-2015, 09:54 AM
  4. Question(s) where in the Arbotix AVR code is it talking to the XBEE serial port?
    By stephen.hazel in forum Arbotix, Microcontrollers, Arduino
    Replies: 5
    Last Post: 05-04-2012, 12:21 PM
  5. Project R2Talk2 - a talking robot with rotating head
    By Macro Man in forum Project Showcase
    Replies: 16
    Last Post: 09-13-2009, 06:45 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •