Results 1 to 3 of 3

Thread: AX12+ instead of AX12A

  1. #1

    AX12+ instead of AX12A

    For these dynamixels, the form factors are different but are they still fully compatible with the existing baritone kits (i.e hexapod with no motors).

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    284

    Re: AX12+ instead of AX12A

    AX-12, AX-12+, AX-18F, AX-12A, AX-18A, AX-12W, and MX-12W have identical external dimensions and mounting systems. There have been some small changes to the design of the horn and mounting flanges to improve structural integrity and reliability, but they do not change their swappable/interchangeable nature in any way. There were significant changes to the gears inside the servos from AX-12+/18F to AX-12A/18A requiring different replacement gearsets, but there were no changes affecting external compatibility.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #3

    Re: AX12+ instead of AX12A

    Thanks for the response, I thought the internals remained the same between the + and A series and that only the external frame was adjusted. I know for the AX12+, getting the M2 nuts to seat in is a painful process.

    ※ AX-12+ is the improved version of existing AX-12; the design of circuit, material, and wheel gear are specially improved.
    ※ AX-12A is a new version of the AX-12+ with the same performance but more advanced external design. Only the AX-12A is now being sold.
    Last edited by ericshi; 10-24-2015 at 07:25 PM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) ax12a troubleshooting
    By tigakub in forum DYNAMIXEL & Robot Actuators
    Replies: 11
    Last Post: 05-15-2015, 04:30 PM
  2. ax12a servos not getting power
    By deathwiz in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 04-13-2014, 06:22 PM
  3. AX12A Baud Rate
    By DVS in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 08-18-2013, 12:44 PM
  4. AX12A sync write
    By DVS in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 08-14-2013, 09:15 PM
  5. Serial Comunication and AX12A
    By DVS in forum DYNAMIXEL & Robot Actuators
    Replies: 0
    Last Post: 07-09-2013, 08:49 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •