Page 2 of 6 FirstFirst 123456 LastLast
Results 11 to 20 of 55

Thread: Camera / Vision Processing (within the HR-OS1 Framework)

  1. #11

    Re: Camera / Vision Processing (within the HR-OS1 Framework)

    hum, and you have done this or are you just saying it should be easy?
    Last edited by LloydF; 09-16-2015 at 09:43 PM.

  2. #12
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,203
    Images
    27
    Rep Power
    268

    Re: Camera / Vision Processing (within the HR-OS1 Framework)

    If you have a 3D printer, it should be trivial to print up a new bracket to mount the shipped USB camera at some angle other than perpendicular to the end of the servo. It will introduce some rotation and translation offsets to the position of the camera relative to the rotational axes of the pan-tilt assembly, but they should be easily handled constants.

    As for the alternate pan-tilt design with a timing belt and pivot, I'm working on a ~2:1 capstan pair for the tilt to do initial testing (300 degrees of servo horn movement into ~150 degrees of camera tilt). If it works anything like I hope, then buying 11T and 21T MXL pulleys and a correctly sized belt would be the next step.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  3. #13

    Re: Camera / Vision Processing (within the HR-OS1 Framework)

    tician, are you a beta tester? Oh yea I see you were having issues with the Arbotix-Pros and Pi's. Yes it seems to be a latency issue with the 3.18 kernel, an real time data. Now I could be wrong but I am pretty sure.
    Last edited by LloydF; 09-17-2015 at 04:05 PM.

  4. #14
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,203
    Images
    27
    Rep Power
    268

    Re: Camera / Vision Processing (within the HR-OS1 Framework)

    Quote Originally Posted by LloydF View Post
    tician, are you a beta tester?
    Not yet, but I have a few years experience building, using, and fixing dynamixel-based robots in addition to the BS EE/ME (and all courses for an MS Engr, but dropped out before finishing my thesis). Lots of ideas pop into my head and reach varying levels of development, but not many ever fully materialize because of limited resources and scary ability to become very quickly bored/disinterested/distracted.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  5. #15

    Re: Camera / Vision Processing (within the HR-OS1 Framework)

    I was Playing with you're rme files, they run on my pi-HROS1. I need to get mine adjusted to carpets, you're get up routines work
    Last edited by LloydF; 09-17-2015 at 04:14 PM.

  6. #16
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    27

    Re: Camera / Vision Processing (within the HR-OS1 Framework)

    Quote Originally Posted by tician View Post
    If you have a 3D printer, it should be trivial to print up a new bracket to mount the shipped USB camera at some angle other than perpendicular to the end of the servo.
    This is true and a note on the subject of the limited downward viewing angle; A little bird has mentioned there will be a (possible?) revision to the HR-OS1 design addressing the issue. I may get impatient and come up with another temporary solution (other than a bigger ball) while we wait.

    Quote Originally Posted by LloydF View Post
    I was Playing with you're rme files, they run on my pi-HROS1. I need to get mine adjusted to carpets, you're get up routines work
    Woooo! That is super cool! What style hands did you have attached to your robot when you tested? BTW, those poses were made with WinRME </shameless plug>

    I'm sure they could be improved upon but at the moment I'm still enjoying them. It's kind of fun to load the ps3 demo and (repeatedly) lay the robot on it's back / belly and watch it get up all on it's own
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  7. #17

    Re: Camera / Vision Processing (within the HR-OS1 Framework)

    I have a shapeways set as there close to indestructible and feather light. Click image for larger version. 

Name:	skinned4port.jpg 
Views:	88 
Size:	117.4 KB 
ID:	6175
    Now that I am on the REAL TIME kernel patch I think I'll name him RT-HROS1.
    Last edited by LloydF; 09-17-2015 at 05:19 PM.

  8. #18
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    27

    Re: Camera / Vision Processing (within the HR-OS1 Framework)

    Cool picture! I like your sign on the wall. When the stand up pages were created I was using the shapeways hands as well. I wonder, especially for standing from a front fall, if the different hands will have a big effect on it's ability to upright. Good to know it works with all the armor attached. I have most of mine off as I'm re-working my bot to keep the weight down.

    Last night I printed a new camera mount that has a 25 degree offset which allows him to see his feet. I hacked up the ps3_demo to add some basic soccer handling and this morning had a little fun...



    There is still much to do! And definitely lots of fun ahead.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  9. #19

    Re: Camera / Vision Processing (within the HR-OS1 Framework)

    Great Film! It gave me a great laugh!

    Kurt

  10. #20

    Re: Camera / Vision Processing (within the HR-OS1 Framework)

    ROFL. So glad yours is as stable as mine, snicker. I think I need a tile soccer sheet, board, poster, to play on.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Remove Compiler Warnings from HR-OS1 framework...
    By KurtEck in forum HR-OS1 Development and Discussion
    Replies: 5
    Last Post: 06-03-2015, 10:44 PM
  2. Raspberry Pi 2 image recovery + HR-OS1 Framework
    By panthallion in forum HR-OS1 Development and Discussion
    Replies: 17
    Last Post: 04-30-2015, 03:36 PM
  3. framework for robotics
    By iacoposk8 in forum Robotics General Discussion
    Replies: 2
    Last Post: 10-11-2013, 07:52 PM
  4. Processing to arduino with key press help
    By jiokl in forum Software and Programming
    Replies: 3
    Last Post: 09-01-2012, 06:19 PM
  5. Theory behind stereoscopic camera vision(?)
    By jrowe47 in forum Sensors
    Replies: 14
    Last Post: 07-20-2008, 05:42 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •