Results 1 to 3 of 3

Thread: Load on a robotic arm

  1. Question Load on a robotic arm

    Hi!

    In order to chose a robot they quantify the load in the datasheet but is that enough to choose a robot? Is it just the weight of the milling head (in my case) that is necessary? I'm still novice in this domain, but I'd think that there is the stress during the milling that I have to consider (which differs with the used material)

    Thanks in advance!

  2. #2

    Re: Load on a robotic arm

    You have to choose at least based on weight of continuous load it can handle, precision of position, and backlash/rigidity.
    Ability to interface with CAM software that you will be using is also a plus :-)

  3. Re: Load on a robotic arm

    Thanks for the reply

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Worried about amp load on some servos
    By contextolibre in forum Power
    Replies: 2
    Last Post: 05-27-2013, 05:17 PM
  2. Question(s) Max amp load on LiPo battery
    By alonso in forum Power
    Replies: 7
    Last Post: 04-06-2013, 02:42 AM
  3. Question(s) Using AX-12's present-load feedback
    By RobotAtlas in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 07-04-2010, 09:33 PM
  4. How much load can a Bioloid hexapod carry?
    By jotheberlock in forum Humanoids, Walkers & Crawlers
    Replies: 21
    Last Post: 02-24-2010, 08:37 PM
  5. Load Cell
    By super-d in forum Sensors
    Replies: 0
    Last Post: 06-05-2009, 11:48 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •