Since getting and assembling my HR-OS1, I've been reading all the previous posts. One that really caught my eye, started by r3n33, made reference to the limited tilt angle that made it impossible for the robot to see it's own feet. Has anyone measured the angle their robot is able to attain? I used to make my own golf clubs and remembered I had a tool for measuring angles, so I dug it out and manged to take some rough measurements.
With the stock build, I am able to look up 22 degrees and down 32 degrees. The up angle would need to be limited even further in actual operation as that is pushing against the cables.
In a reply at the bottom of page 1 of that thread, tician hinted at using a C-bracket and a redesigned P1. I've made a mock up and boy what a difference! Using a Biloid F1 bracket with the angled arms going up and forward, I can get 90 degrees up and 110 degrees down! Does require flipping servo 19 to horn up instead of horn down.
I just finished printing r3n33's Chappie head, (thanks for the files) and with it on the same mockup I can still get 90 degrees up, but only 47 degrees down. The extra thing under Chappie's chin limits downward travel. Using the Chappie head would require both servos to be on top of the P1 plate. Without it, the pan servo could go on the bottom side of the P1 plate.
Gotta print a red antenna as the orange one just doesn't look right.
I'm about 80% done on designing both types of P1 one plates I need, then 3D print and try them out. Gotta see what I can come up with for a thrust bearing.
Bookmarks