Page 2 of 2 FirstFirst 12
Results 11 to 15 of 15

Thread: Dynamixel MX-12W with Arbotix-m dead zones

  1. #11
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    39

    Re: Dynamixel MX-12W with Arbotix-m dead zones

    Good point. Have you adjusted or tried changing the default PID values?
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  2. Re: Dynamixel MX-12W with Arbotix-m dead zones

    Quote Originally Posted by r3n33 View Post
    Good point. Have you adjusted or tried changing the default PID values?
    No I have not, since there is no load applied to the servo I assumed the default values would suffice.

  3. Re: Dynamixel MX-12W with Arbotix-m dead zones

    Ok so messing with my MX-12W Dynamixel I have noticed a little slack in the horn. When the motor is on and I am sitting in a while loop, printing the present position every second, with little to no force I can move the horn back and forth in the slack range and it will update my position. The slack range is approximately 5 positions.

    As mentioned earlier by tician and r3n33, I think there is a PID solution. I don't see a lot of information on the e-manual about setting the PID values except the default values are as followed: P = 8; I = 0; D = 8. I'm nervous I am going to mess something up because I am using this motor in a project and I will not have enough time to replace it by the end of the semester.

    Any guidance besides a wiki page to what PID means would be more than appreciated.

  4. #14
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    39

    Re: Dynamixel MX-12W with Arbotix-m dead zones

    Yep tician lives up to the title.. like google but for robots He's pretty sharp! ... and probably could do a better job explaining PID but I'll give it a try.

    P is the proportional gain relative to the error at the time of the reading. This is typically the main driving force of a PID controller. Too low of a value and the goal position may never be reached. Too high of a value the goal position will be reached but overshot.. causing an oscillation.

    I is the integral term which is applied to the error over time. It can help a PID controller reach the goal quickly and can also be used to compensate for a persistent error offset. This term isn't always necessary for decent PID control which is likely why it's 0 by default. In your case this is the term I'd try increasing slowly to help your situation (small error of 1-5).

    D is the derivative gain which is applied to change in error since the last reading. This can have a couple effects. One it will "slow" or decrease the controller's output as the goal position is approaching. On the other side of things it can also drive the output quickly toward the goal position if the error is increasing.

    PID tuning can be tricky. Sometimes a PID tune will work for one situation but not another (differences in load, external disruption, etc.). I'd recommend trying to increase the P gain slightly or the I gain at first. Keep in mind PID is like a balance game.. changing one value may require another to change for good output.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  5. #15

    Re: Dynamixel MX-12W with Arbotix-m dead zones

    As I mentioned, I have 1 MX-12, so thought I would do a quick and dirty test... I ran the test on my Odroid XU4 with an USB2AX in it and hacked in a simple pan test into my Raspberry Pi test AX servo program... I have not updated my project on github with this, but the code looks like:
    Code:
    void PanServoTest(void) {
        unsigned long ulBefore;
        unsigned long ulDelta;
        word wID;
        int start_pos;
        int  end_pos;
        int Pos;
        int cur_pos;
        int cur_speed;
        int servo_increment = 1;
        int loop_count;
        word w;
        int dxl_result;
    
        if (!FGetNextCmdNum(&wID))
            return;    // no parameters so bail.
    
        if (!FGetNextCmdNum(&w))
            return;    // no parameters so bail.
        start_pos = (int)w;
    
        if (!FGetNextCmdNum(&w))
            return;    // no parameters so bail.
        end_pos = (int)w;
    
        if (FGetNextCmdNum(&w))
            servo_increment = (int)w;
    
       
        printf("Servo %d Pan test %d - %d step %d\n", wID, start_pos, end_pos, servo_increment);
        
        ax12SetRegister2(wID, AX_GOAL_POSITION_L, start_pos); 
        delay(200); // give some time to get there!
        
        if (start_pos > end_pos)
            servo_increment = -servo_increment; 
    
        for (Pos = start_pos; ; Pos += servo_increment) {
            if ( ((servo_increment > 0) && (Pos > end_pos))
                    || ((servo_increment < 0) && (Pos < end_pos)) )
                break;
            ax12SetRegister2(wID, AX_GOAL_POSITION_L, Pos);
            dxl_result = dxl_get_result();
    
            // Lets wait until we get there
            for (loop_count = 0; loop_count < 50; loop_count++)
            {
                delay(10);
                cur_pos = ax12GetRegister(wID, AX_PRESENT_POSITION_L, 2 );
                if (cur_pos == Pos)
                    break;
            } 
            if (cur_pos != Pos) {
                cur_speed = ax12GetRegister(wID, AX_PRESENT_SPEED_L, 2 );
                printf("    Goal: %d Actual: %d Speed: %d res=%d\n", Pos, cur_pos, cur_speed, dxl_result);
            }
        }
        printf("Completed\n\n");
    }
    Please pardon that as I said this is Quick and dirty!.
    The test program has a real simple command line UI,
    Sample run:
    Code:
    [email protected]:~/Raspberry_pi/AX12_Test$ ./AX12_Test
    Start
    Controller model 4201 on fd(253)
    System Voltage in 10ths: 123
    0 - All Servos off
    1 - All Servos center
    2 - Set Servo position [<Servo>] <Position> [<Speed>]
    3 - Set Servo Angle
    4 - Get Servo Positions
    5 - Sync Read Servo positions
    7 - Set Servos return delay
    8 - Set ID: <old> <new>
    9 - Print Servo Values
    t - Toggle track Servos
    w - write <servo> <reg> <val> (can be multiple values...
    p - Pan servo start end step
    h - hold [<sn>]
    f - free [<sn>]
    :p 1 1000 4000 100
    
    Servo 1 Pan test 1000 - 4000 step 100
        Goal: 1000 Actual: 1016 Speed: 0 res=1
        Goal: 1200 Actual: 1198 Speed: 0 res=1
        Goal: 1400 Actual: 1399 Speed: 0 res=1
        Goal: 1500 Actual: 1501 Speed: 0 res=1
        Goal: 1700 Actual: 1698 Speed: 0 res=1
        Goal: 1800 Actual: 1798 Speed: 0 res=1
        Goal: 1900 Actual: 1898 Speed: 0 res=1
        Goal: 2000 Actual: 1996 Speed: 0 res=1
        Goal: 2200 Actual: 2203 Speed: 0 res=1
        Goal: 2300 Actual: 2296 Speed: 0 res=1
        Goal: 2400 Actual: 2398 Speed: 0 res=1
        Goal: 2500 Actual: 2497 Speed: 0 res=1
        Goal: 2600 Actual: 2596 Speed: 0 res=1
        Goal: 2700 Actual: 2696 Speed: 0 res=1
        Goal: 2800 Actual: 2794 Speed: 0 res=1
        Goal: 2900 Actual: 2896 Speed: 0 res=1
        Goal: 3000 Actual: 2996 Speed: 0 res=1
        Goal: 3100 Actual: 3097 Speed: 0 res=1
        Goal: 3200 Actual: 3196 Speed: 0 res=1
        Goal: 3300 Actual: 3296 Speed: 0 res=1
        Goal: 3400 Actual: 3396 Speed: 0 res=1
        Goal: 3700 Actual: 3696 Speed: 0 res=1
        Goal: 3800 Actual: 3795 Speed: 0 res=1
    Completed
    So for this run I had the servo move 100 units at a time from 1000 to 4000, and tried to read the Current position back in up to 50 times until servo position matched... Disregarding the first one, where maybe I should have let the servo have some more time to settle in position, you can see there were several of these runs where the servo was off by a few...

    Now back to my other playing.

Thread Information

Users Browsing this Thread

There are currently 2 users browsing this thread. (0 members and 2 guests)

Similar Threads

  1. PID Control for Dynamixel servos using Arbotix-M
    By navidahmeduom in forum Arbotix, Microcontrollers, Arduino
    Replies: 6
    Last Post: 05-20-2015, 11:15 AM
  2. Project Biped Robot with Arbotix + Dynamixel AX-12A
    By kanuto in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 11-09-2014, 05:58 PM
  3. troubleshooting a dynamixel.. Possible dead MX-28?
    By wthierry in forum DYNAMIXEL & Robot Actuators
    Replies: 10
    Last Post: 08-28-2014, 12:33 PM
  4. Question(s) Arbotix-M sketch for dynamixel AX-12A's
    By ABB in forum Software and Programming
    Replies: 2
    Last Post: 03-03-2014, 06:33 AM
  5. 18 Dynamixel Ax-12A with ArbotiX/Arduino - How to connect the dynamixel?
    By Snuuq in forum Arbotix, Microcontrollers, Arduino
    Replies: 20
    Last Post: 02-14-2014, 12:29 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •