Hey guys,
Robotis announced a few days ago at Robotworld 2015 their new Dynamixel servos : XM-430.
They are pretty different from the previous ones, from a mechanical perspective.
From the top of my head before I take some time to make a full review:
- the idler design can let one cable get out of the servo on the rotation axis, or can be replaced by a cap if not needed.
- case is mostly metal, with a few M2.5 threaded holes (4 on the sides and bottom, 2 front). No flanges, it's a parallelepiped.
- size is smaller than MX-64
- two choices of gear sets: one for speed, other for torque (about 50kg.cm iirc).
- 12V, RS485 but with new type of connector. Electrically compatible with previous MX-R series.
- they finally put a switching regulator to power the control electronics
- can talk either Dynamixel Protocol 1.0 or 2.0, it can be set in the control table.
- resolution seems to be the same as MX series (12 bits, 4096) but if needed it can be divided in firmware to use it as if 10bits, 1024.
- intended price is still unknown but hoped to be not too much above MX-28.
- release date unknown.
I'll get you a more comprehensive review of the thing later - I still have some demos to do at IEEE Humanoids with the robot I worked on for the MiniDRC event organized by Robotis - and for which we used 20 of these to make a Darwin-size rescue robot (I'll post about that too).
My experience so far is only with the Speed version. Pretty nice feeling, it makes me think of an MX-28 with more torque.
We've had a problem when the robot fell from about 15-20 cm high while all the joints were powered: the knees took a bad hit, and the shaft of both of them got a bit twisted (a few degrees) between the output gear and tip of the output shaft . I imagine (hope) they will fix that before release.
If you have specific questions, don't hesitate and I'll try to get you an answer.
![]()
Bookmarks