Results 1 to 1 of 1

Thread: Dynamixel RX-24F with MAX485

  1. #1
    BrechtW Guest

    Question Dynamixel RX-24F with MAX485

    I'm using this arduino and I want to control the RX-24F.

    I'm using the shematic provided here. http://support.robotis.com/en/techsu...ies/rx-24f.htm. I used the dynamixel library dynamixelSerial form Savage Electronics (http://sourceforge.net/projects/dyna...?source=navbar)

    I set the baudrate to 57600.

    https://goo.gl/photos/n7QxG2Dm6eUayMHn7

    The images are a scoop image and the setup (arduino is not connected when taking a picture).

    Do I need extra resistors with D+ and D-?.
    Last edited by BrechtW; 11-08-2015 at 03:18 PM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Just For Fun Arduino Dynamixel RS485 using Max485 module
    By Jim Cheong in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 10-21-2015, 11:13 AM
  2. Arduino Library for Dynamixel XL-320 (and Dynamixel PRO if modified).
    By LuisGIII in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 06-08-2015, 12:00 AM
  3. 18 Dynamixel Ax-12A with ArbotiX/Arduino - How to connect the dynamixel?
    By Snuuq in forum Arbotix, Microcontrollers, Arduino
    Replies: 20
    Last Post: 02-14-2014, 12:29 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •