Results 1 to 3 of 3

Thread: OpenCM 9.04 - B and 18 Dynamixel AX-12A servos

  1. OpenCM 9.04 - B and 18 Dynamixel AX-12A servos

    Hi,

    I'm building a Bioloid Type A robot. But I want to control it using theOpenCM 9.04-B controller.

    My idea is to use the four TTL pins for servos. In each pin I'm thinking to connect 5 or 6 servos (AX-12A) in serial mode.

    For the moment I don’t have any battery, so I'm going to connect the + and - pins of the OpenCM to an 11 V power supply.

    It would work or the controller will be damaged?

    Thanks and sorry for my bad English, I'm learning it.
    Last edited by OpenRobot; 11-29-2015 at 06:02 PM.

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,286
    Images
    27
    Rep Power
    275

    Re: OpenCM 9.04 - B and 18 Dynamixel AX-12A servos

    It is perfectly safe, but the power traces of the OpenCM are meant for the low-power XL-320 servos in the Darwin-Mini, so they are not able to handle very much current (the two pin JST connectors are rated ~2A, where AX-12 can require 1A each during higher loading). The AX/TTL powered hub from the trossen shop would be a better way to power everything (including the OpenCM connected by one 3-pin dynamixel cable to the hub) as screw terminal and barrel connector mean that no special dynamixel cables need to be created to connect the power supply (battery) to the servos. If you do not want to make an adapter cable for the battery to connect it to the hub, trossen shop also sells a cable harness ready to use to connect Deans/T-connector equipped batteries - like those sold in the trossen shop - and a barrel connector for the hub.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  3. Re: OpenCM 9.04 - B and 18 Dynamixel AX-12A servos

    Thank you so much for your explanation.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. New Dynamixel servos: XM-430
    By Xevel in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 12-15-2015, 02:02 PM
  2. Darwin Mini / OpenCM 9.04 power-on trouble
    By jwatte in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 07-27-2015, 12:16 AM
  3. Question(s) Control AX/RX Dynamixel with Roboplus task with OpenCM9.04 type C + OpenCM 485 EXP
    By kongguan in forum DYNAMIXEL & Robot Actuators
    Replies: 0
    Last Post: 04-22-2015, 05:21 AM
  4. Dynamixel Manager cannot find servos
    By lukeyes in forum DYNAMIXEL & Robot Actuators
    Replies: 30
    Last Post: 10-29-2014, 03:43 PM
  5. Question(s) Wheels for Dynamixel Servos
    By SamQ in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 07-27-2011, 08:56 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •