Page 2 of 4 FirstFirst 1234 LastLast
Results 11 to 20 of 32

Thread: The New PhantomX AX Metal Hexapod Kit is here!

  1. #11
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    41

    Re: The New PhantomX AX Metal Hexapod Kit is here!

    Quote Originally Posted by wadecore View Post
    The total weight for the MK-II came in around 4.4 lbs. The new MK-III kit (mind you with a huge battery that fills the entire body cavity) comes in at 5.1 lbs. It feels like a tank, but moves as smoothly as ever.
    Thanks Do you have any pictures of the new toe design? I'm curious if it still uses the stick on rubber pads for traction? Or if I could possibly print a rubberized toe to replace the delrin plate.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  2. #12
    Join Date
    Mar 2015
    Location
    Downers Grove, IL
    Posts
    22
    Rep Power
    23

    Re: The New PhantomX AX Metal Hexapod Kit is here!

    Quote Originally Posted by r3n33 View Post
    Thanks Do you have any pictures of the new toe design? I'm curious if it still uses the stick on rubber pads for traction? Or if I could possibly print a rubberized toe to replace the delrin plate.
    I'm sure you've seen it by now, but I took a video of the new foot. The delrin plate is slotted so that you can place rubber socks over it. This really keeps things running super smooth. It grips enough to move cleanly on hard surfaces, and it doesn't have so much surface area that it causes an issue on carpet. Always feel free to experiment with the design. You might find out something that we haven't!
    https://www.instagram.com/p/-2XVz2Hg1O/

  3. #13
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    41

    Re: The New PhantomX AX Metal Hexapod Kit is here!

    Thanks Wade! I think the new foot looks great and bet it will withstand a lot more wear and tear.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  4. #14

    Re: The New PhantomX AX Metal Hexapod Kit is here!

    Yea! I love the metal parts, I had stopped working on this bot because the plates would get brittle and break when you chnaged
    things out. No more. Good job thank you.

  5. Re: The New PhantomX AX Metal Hexapod Kit is here!

    Hello!

    As I can see, the junction between the tibia bracket and the servo has only 4 screws per side, and in the mark II version it had 7, with one of the sides of the bracket extending the full extension of the servo. As the servo attahcment is made of plastic, would not have been better to design that part of the servo as the previous version? Or is this enough for the weight it has to support? I'm thinking about the long term use and possible problems in the future.

    Anyway, great update for the PhantomX!

    Alex

  6. #16

    Re: The New PhantomX AX Metal Hexapod Kit is here!

    While the servo is made of plastic, it's made of a much stronger plastic than the one used in the previous Phantom cases.

    Sincerely,

    jw

  7. Re: The New PhantomX AX Metal Hexapod Kit is here!

    Thank you jw. Glad to see the Servos are also improved in the new version!

    I have a question I don't know if someone will know about it: looking at the original PhantomX, the one with the straight tibias, I see that the design of the legs is very different from the mark II and III, and somehow it likes me more, but I suppose that the new design offers some advantages to the hexapod, but I don't know clearly what are them. Anyone knows what benefits (or reasons for the change) has the mark II leg design over the original PhantomX?

    Thank you

    Alex

  8. #18

    Re: The New PhantomX AX Metal Hexapod Kit is here!

    Glad to see the Servos are also improved in the new version!
    Sorry, I was unclear. It turns out that different kinds of plastics have different properties.

    The servos haven't changed. They're made of something like Acetal, which is a strong, robust plastic. (I haven't found publicly available specs, but it feels like Acetal in the hand, and it's less slippery than something like Nylon 6/6, which is another strong engineering plastic, and less shiny than something like ABS which is cheaper, but less robust, which kind-of leaves Acetal as the main candidate.)

    The previous version of the skeleton used an Acrylic/Polycarbonate mix that was laser cut. Unfortunately, that's somewhat fragile and sesitive to cracking. But it's easy to laser cut and manufacture things out of!

    The new version is apparently made of 5052 aluminum. My guess is they water jet cut it, and then bend some pieces on a break. 5052 is a little more wiggly than 6061, but it bends much nicer without cracking, and it is a significant upgrade compared to the previous plastics!

    Also, I want a quad version :-)
    Last edited by jwatte; 02-05-2016 at 10:30 PM.

  9. #19

    Re: The New PhantomX AX Metal Hexapod Kit is here!

    nice, tempting

  10. #20

    Re: The New PhantomX AX Metal Hexapod Kit is here!

    Quote Originally Posted by ezex View Post
    nice, tempting
    I broke down and ordered...

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX Hexapod Kit
    By SuperMiguel in forum Projects For Request and/or Sale
    Replies: 12
    Last Post: 12-29-2013, 09:36 PM
  2. Question(s) PhantomX Hexapod with AX-18
    By Jim Cheong in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 06-19-2013, 07:57 PM
  3. For learning: PhantomX Hexapod vs PhantomX Quadruped
    By Leugim in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-26-2012, 08:50 AM
  4. My PhantomX Hexapod
    By Gilrock in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 09-26-2012, 02:23 PM
  5. PhantomX Hexapod and Bioloid
    By billyzelsnack in forum Garage Sale
    Replies: 3
    Last Post: 08-08-2011, 07:20 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •