Results 1 to 2 of 2

Thread: What do small electronics use instead of arduino?

  1. What do small electronics use instead of arduino?

    I have used arduino for many small projects and I began to wonder what companies producing small electronics use as the brains for it. Its not like they are stuffing an arduino board into them. I have an arduino project im working on that uses an led to signal status, a laser diode, and a photo resistor. If this were to be turned into a small electronic, what would be used? Obviously, the photo resistor, led, and laser diode would be used but how would it all go together without an arduino to do the brain work. when the photo resistor sees the laser, it turns on the led. Just curious how things are done in the real world. Thanks for any insight.

  2. #2

    Re: What do small electronics use instead of arduino?

    The Arduino board contains a number of things:

    1) A microcontroller chip.
    2) The large DIP package of the microcontroller chip (the 28-pin IC you can remove and/or replace on Arduino Uno boards)
    3) Interface electronics to let you program the chip, interface with the world, power it from various voltages, etc.
    4) A lot of empty space, for "historical" reasons.

    If you just need to drop a microcontroller into a design, you'd typically use the same kind of microcontroller chip, but in a smaller package (anything from TQFP to chips epoxied straight onto circuit boards.) You'd also typically use a little bit of surface-mount voltage regulators to power it, and whatever else is needed to interface with whatever the chip is talking to.

    Also, the AVR microcontroller is okay for a small 8-bit microcontroller; it's very easy to program even at the register/device level (without using the Arduino libraries.) However, there are many other microcontroller "families" -- the most common one is ARM, which has a small version (Cortex M0 through Cortex M4) that can be both cheaper and higher performance than the AVR. And, as a bonus, it's the same kind of CPU as found in cell phones (Cortex A54 and such) so they can share more tools and libraries.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Is there an HR-OS5 electronics kit for those who already own Dynamixels?
    By robot_yan in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 12-24-2014, 08:37 AM
  2. New to electronics, looking for help on my project!
    By Architeuthis in forum Robotics General Discussion
    Replies: 0
    Last Post: 03-31-2012, 11:57 AM
  3. Lynxmotion Electronics
    By Quantum in forum Garage Sale
    Replies: 1
    Last Post: 01-20-2010, 08:28 PM
  4. Learning Electronics
    By jes1510 in forum Robotics General Discussion
    Replies: 12
    Last Post: 12-06-2008, 12:12 AM
  5. Project Arduino and RSRs (Really Small Robots)
    By LinuxGuy in forum Rovers
    Replies: 8
    Last Post: 08-12-2008, 03:36 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •