We (R-Team) got the go ahead from Andrew (from Trossen) and Dave Calkins (from Robogames) to host the Mech Warfare event for 2016.
First we would like to get an indication on who thinks they will be able to make the event this year. (High Probability or Maybe). R-Team robotics will be showing up enforce. The event is just over two months away, so you really need a functioning or near functional mech at this time to make it.
Here are some of our thoughts.
A) The ruleset will be a reuse of the 2013 ruleset as close as possible. There will be no Hardcore League this year.
B) All mechs will be guaranteed at least two matches. We will structure the match play based on the number of Mechs qualified to maximize the number of matches that everyone gets. .
C) The Mech's will have to qualify, either live at the event or through video (preferred)
D) There are 3 acceptable scoring panels that will be accepted. 1) The Trossen FSR panels from past years. 2) The R-Team Piezo Panel 3) the Boston variant of the R-Team piezo panel. All of these have been verified to be functionally equivalent. There may be slight performance differences between these panels, but at this time we have not verified if any give an advantage. The Trossen scoring Transponder from past years will be used and all panels must be compatible with it. Since the event is so close we are assuming any mech competing is an existing mech and most likely already has one of these scoring systems. We can come up with a small amount of scoring panels/transponders/LED boards if someone is needing them.
E) We highly recommend the 5.8GHz Analog Video cameras. It really is a much more enjoyable experience. Due to the short timeframe we won't enforce this, but in the future it will most likely become part of the ruleset. We will provide a wireless router solution for those w/o 5.8Ghz cameras and will be working this over the next couple of months.
F) The arena is 15'x15'. The buildings are 3'x3' (which is slightly larger than previous years). Currently the buildings are all identical so it can get a bit disorienting on your location. We may add some identifying marks to the arena to help.
G) Currentyy there isn't a registration for thr Mech Warfare event yet on the Robogames website. Hopefully that will be soon but can't guarantee any date. In the mean time, get your Mechs ready!
Bookmarks