Page 1 of 2 12 LastLast
Results 1 to 10 of 11

Thread: What programming editor do you recommend?

  1. #1

    What programming editor do you recommend?

    Just wondering what editors are people using these days for projects like the HROS1 and the like.

    On Windows I have been mostly using Programmers Notepad for these types of projects, likewise for when I am editing libraries for Arduino... I have used this one for awhile now and it is not bad, but there are times when it is a bit limited, and I bit frustrating when you have lots of source files... Back a long long time ago, when I was working I used to use Visual Slickedit, but have not had a copy of that for a very long time.

    I have some other editors installed as well, such as ones based on Microsoft Visual studio, which I use at times... Just wished it loaded a lot faster. Also have at least one copy of Eclipse installed (for Edison)... I have also used Geany...

    Currently on the Mac I have Geany, Chicken and TextWrangler installed.

    So this morning when I got a bit frustrated trying to keep several sets of files open, with over 20 some files open. This included many of the files in the HROS1-Framework, both Framework and Linux specific files, as well as files from my Raspberry Pi project, it made me wonder if maybe I should use a different editor...

    Suggestions?

  2. #2

    Re: What programming editor do you recommend?

    When I use things integrated with Arduino, I just use the (terrible, terrible) Arduino editor. Going with the flow leads to less pain over time; trying to customize everything just ends up wasting time.
    When I edit random files on Windows, I use Notepad++.
    When I write code on Windows for real, I use Visual Studio if at all possible. (Like, I have a compatibility layer that lets me build Arduino sketches in Visual Studio with fake hardware inputs, so I can debug them!)

    When I'm on Linux, I use vim and make. And, honestly, that's about as good as using Visual Studio on Windows, except the GDB user experience is terrible.

  3. #3
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    282

    Re: What programming editor do you recommend?

    I've not used it much yet, but sublime text seems quite nice. r3n33 brought it up in your PuTTY thread a while back. Gives me the familiar feel of gedit with the ability to quickly open multiple files via projects. Also has some build capabilities that I've not tried out yet. Have not bought a license yet, but likely will if do completely switch from gedit.

    Took a little while to get the layout like I wanted because of the minimap size not really being easily/(at all?) modifiable and it was refusing to fit a full 80 character line without a horizontal scroll bar in a single half-screen window like gedit. Changing text settings to match gedit and changing gutter margin to -15 finally fixed that.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  4. #4
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    39

    Re: What programming editor do you recommend?

    My vote is still for Sublime Text. It is full of features that I find useful and my license works on the osx, windows, linux versions which makes it nearly seamless between machines. I can also say I've never had an issue with lots of open files or any performance quirks. I believe the free version gives you the full feature set with a concentration killing message box that reminds you they'd like some money.

    Notepad++ is also one of the editors I like on Windows but since I purchased Sublime I haven't had the need for anything else.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  5. #5

    Re: What programming editor do you recommend?

    Thanks,

    Sounds good. I downloaded it and will try it.

  6. #6
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    860
    Images
    25
    Rep Power
    93

    Re: What programming editor do you recommend?

    +1 on sublime as well.

  7. #7
    Join Date
    Mar 2015
    Location
    Downers Grove, IL
    Posts
    22
    Rep Power
    21

    Re: What programming editor do you recommend?

    I'm gonna throw in another +1 for Sublime. I use it on Windows and Linux. It's sexy.

  8. #8

    Re: What programming editor do you recommend?

    I do most all of my programming with vim. The neat thing about using it for hr-os1 or other small computer projects is that it's included with most all Linux distros by default. Just ssh to the device and type 'vi'. One term window for the editor and a second for the compiler. Can't get better than that.

  9. #9

    Re: What programming editor do you recommend?

    Thanks, I have been known to do that in a pinch, but vi is not my favorite editor, especially if I am doing things like, working through all of the files associated with talking the the Arbotix Pro across multiple directories... I have even used nano before, but...

    I do have Sublime Text installed now and have done a little playing around. Luckily most of the key bindings are pretty close to most of the other editors. Have not tried to do anything fancy yet, like figure out if there is a good way to jump from a function call in the code to find where it is defined in header and implementation... I think there are some ctags like extensions...

    Jwatte: I also use Arduino IDE when doing Arduino stuff. It is not great, but at least they have added a few things now, like being able to jump to a line number... Wish they also had support to edit libraries... But...

  10. #10

    Re: What programming editor do you recommend?

    working through all of the files associated with talking the the Arbotix Pro across multiple directories
    In your .vimrc:
    set hid

    this keeps all the other files in RAM when switching to a new file.
    You might as well also add:

    set ic
    set autoident
    set expandtab
    set sw=4
    set background=light
    set t_Co=256
    colorscheme biogoo


    Separately, commands like:

    :grep -r foo . --include=\*.h

    This will grep for foo in all the files with a .h extension. (I'm sure this is also mapped to some shorter key in some setups)
    You then move through the hits with ":cn" and ":cp" (which you can map to <F6> and <F7> for example)

    Other cool commands include ":bel spl <filename>" to open a new file in a second horizontal tab, and "%s/regex/replacement/g" to global search-and-replace in the current file. Also, uppercase marks ('A to set, mA to go to) are great when working in many files!

    I'm the first to admit that vim does take a willingness to work at it to get proficient in; for me it does pay off on the other side of the learning curve.
    Last edited by jwatte; 02-08-2016 at 12:07 PM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Replies: 6
    Last Post: 12-31-2015, 11:24 AM
  2. Replies: 1
    Last Post: 05-30-2013, 07:42 AM
  3. commander code editor
    By abdelrahman in forum ROS - Robot Operating System
    Replies: 7
    Last Post: 02-14-2013, 02:09 AM
  4. Project Z pad++ C/C++ editor
    By SvenStrikesBack in forum Software and Programming
    Replies: 0
    Last Post: 02-02-2011, 11:09 PM
  5. Bioloid RoboPlus Motion Editor
    By herman2992 in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 01-14-2011, 08:16 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •