Results 1 to 2 of 2

Thread: Jetduino: Robotics interface for NVIDIA Jetson TK1

  1. Jetduino: Robotics interface for NVIDIA Jetson TK1

    I have been working on a new interface board for the Jetson TK1 embedded supercomputer called the Jetduino. It makes it very easy to build robots that can use the parallel processing capabilites of the NVIDIA GPU for vision and neural neural networks.

    Click image for larger version. 

Name:	YouTubeCover.jpg 
Views:	203 
Size:	77.7 KB 
ID:	6442Click image for larger version. 

Name:	Jetduino_Front_small.jpg 
Views:	250 
Size:	92.2 KB 
ID:	6443


    The Jetduino mounts above the Jetson and has a small connector that fits in the 2mm J3A connectors. A Raspberry Pi GPIO ribbon cable then connects it to the Jetduino. It has mounting points for a 2.5" HD, wireless antennas, a large proto-typing area, and a built-in shield for an Arduino Due. Just like the GrovePi for the Rapsberry Pi, you can use Python and C libraries to talk directly to the Arduino to set and receive digital and analog data. You can also control regular and smart servos. It has numerous Grove and RobotGeek connectors for modular sensors and motor actuators. I just put out a new blog post and two YouTube videos showing how to setup the Jetduino and perform digital I/O with 12 of the Jetson TK1 GPIO lines, and the 54 lines available on the Due. I am working on videos to show off the other features as well. If you would like to be notified when these are available please sign up for my newsletter. I plan to launch a crowdfunding campaign to get the Jetduino produced sometime in March or April, and I will need the help of any makers out there who want to make it easier to build robots or electronic projects with the awesome Jetson TK1.


    Blog Post with YouTube videos: http://neurorobotictech.com/Communit...and-digital-IO
    Newsletter: http://neurorobotictech.com/Community/Newsletter


    Here are a couple of links describing what the Jetduino is.
    Jetduino V1 description: http://neurorobotictech.com/Communit...boards-ordered
    Jetduino V1 test results: http://neurorobotictech.com/Communit...1-Test-Results


    Thanks
    Attached Thumbnails Attached Thumbnails Click image for larger version. 

Name:	Jetduino_SmallCombined.png 
Views:	105 
Size:	243.4 KB 
ID:	6441  

  2. #2
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    28

    Re: Jetduino: Robotics interface for NVIDIA Jetson TK1

    Cool! If I was working with a TK1 I'd definitely try this.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Interesting RX-28M with TTL interface & 12V
    By RobotAtlas in forum DYNAMIXEL & Robot Actuators
    Replies: 7
    Last Post: 05-16-2011, 11:22 AM
  2. phidget LCD interface kit
    By Adam in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 06-07-2010, 08:58 PM
  3. SRV-1 Custom USB Interface
    By middleton.s.a in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 03-01-2010, 02:22 PM
  4. nvidia Tegra for $99!
    By billyzelsnack in forum Robot Computers
    Replies: 0
    Last Post: 02-17-2009, 12:01 PM
  5. interface cable
    By chocobot in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 04-10-2007, 11:04 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •