Results 1 to 2 of 2

Thread: Chip Quik Low-Temp Lead-Free Solder Paste (Sn42/Bi57.6/Ag0.4)

  1. #1
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,315
    Images
    27
    Rep Power
    279

    Chip Quik Low-Temp Lead-Free Solder Paste (Sn42/Bi57.6/Ag0.4)

    GREATEST. STUFF. EVER.
    ...as long as you do not need guaranteed survival at automotive temperature ranges (melts at 138*C).

    It is easily reflowed by a Sparkfun Heaterizer and can remain molten for several seconds after removing heat. Had to reflow the tiny SOT-563 ESD/EMI chip for the DXL buss a few times on both the ShInDy and transponder boards because I did not get the stencils seated quite right*, but no dead chips or melted plastic.

    *Combination of tiny boards with SMD pads to very near most of the outer edges, not bothering to build jigs to ensure alignment, and the kapton stencils curling upward a bit (cut from rolls of film).
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  2. #2

    Re: Chip Quik Low-Temp Lead-Free Solder Paste (Sn42/Bi57.6/Ag0.4)

    Nice! Like Fields' metal, but without the Indium :-)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Free color solder mask choice at Elecrow
    By click in forum Garage Sale
    Replies: 0
    Last Post: 01-11-2013, 09:00 AM
  2. please lead me to work with rfid
    By unforgiven in forum Project Showcase
    Replies: 0
    Last Post: 07-24-2012, 07:22 AM
  3. 12V Lead Acid Battery Desulfator
    By avayan in forum Power
    Replies: 3
    Last Post: 10-12-2009, 07:02 AM
  4. Discussion Chip of choice?
    By kankatee in forum Robot Computers
    Replies: 24
    Last Post: 12-16-2008, 04:12 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •