Results 1 to 4 of 4

Thread: dxl_monitor Access or Range Error

  1. #1
    Fredenburger Guest

    dxl_monitor Access or Range Error

    Hello all,

    I am working on HR-OS1. Yesterday I noticed his right leg wasn't moving. I tested it on dxl_monitor, and servos 11 and 15 didn't work. When I try to use wr 30 [any number], any servo will move except these two. The message I get back says "Access or Range Error!", unless I use wr 30 0, which just does nothing. Does anyone know how to help? Thanks!

  2. #2

    Re: dxl_monitor Access or Range Error

    Do they respond to ping? Did they lose their IDs?

  3. #3
    Join Date
    May 2014
    Location
    Carlsbad, CA
    Posts
    31
    Rep Power
    16

    Re: dxl_monitor Access or Range Error

    Do you have a Robotis USB2Dynamixel device? If so, download the Robotis RoboPlus software.
    Isolate the questionable servos, plug 1 into the USB2Dynamixel, follow the directions in the Dynamixel Wizard.
    You might need to do the 'Dynamixel Firmware Recovery'. Then you can re-assign the ID number.
    I have recovered the use of several AX-12s this way.

    Good luck.

    BTW - The USB2Dynamixel is very useful if you plan to use/maintain AX-12s and a number of replacement gear sets is almost a must have.

  4. #4

    Re: dxl_monitor Access or Range Error

    What I would often do, is to do some simple tests to see if by chance some of these servos reset their ID to servo #1...

    Have been hit more than once on the PhantomX and HROS1...

    Note: I most often use some of my own test programs, like the ones I have in my Raspberry Pi project, but also do most of this with the dxl_monitor program.

    Simple test: if load dxl_monitor
    set the id to talk to servo #1 and now tell servo #1 to move to some new position, lets say 600. If the servos that were not responding move, they probably have servo address 1.
    Code:
    [ID:200(ARBOTIX_PRO)] id 1
    [ID:1(R_SHOULDER_PITCH)] wr 30 600
     Writing successful!
    if this happens you can also probably use the dxl_monitor to renumber them again. It is sort of a pain, but you need to then isolate each of the servos that have reset (as well as the real #1), example unplug the AX servos going to the right shoulder such that real #1 is not plugged in aslo then unplug somewhere in the right leg below hip.
    Then only the right hip should respond to commands to servo #1.

    So then do something like: Note: this is assuming you still have ID:1 selected, if not issue the ID command
    Code:
    wr 3 11
    Which should hopefully now have the right hip back. So plug the cable back into the lower right leg and repeat except, set the appropriate id maybe
    Code:
    wr 3 15
    Plug the shoulder back in and do a new scan to see if all of the servos now show up.

    Good luck.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Compiling Error with Arduin IDE / Pypose : could not read servo error
    By lweydert in forum Software and Programming
    Replies: 3
    Last Post: 03-27-2013, 08:16 AM
  2. Open Access Publishing (Free Books)
    By jdolecki in forum Robotics General Discussion
    Replies: 1
    Last Post: 08-20-2012, 07:58 AM
  3. Discussion Location Tracking Using 802.11 Wireless Access Points
    By Asimovian in forum Software and Programming
    Replies: 11
    Last Post: 03-25-2012, 10:57 PM
  4. Access Denied to Port??!!
    By cloud_skyblue in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 08-23-2010, 09:14 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •