Results 1 to 2 of 2

Thread: IMU support - Next gen Arbotiix Pro/ or Playing with my Teensy version of Arbotix-pro...

  1. #1

    IMU support - Next gen Arbotiix Pro/ or Playing with my Teensy version of Arbotix-pro...

    Just wondering if anyone has done much playing around with using some form of IMU with their HROS1 or HROS5 robots, instead of relying on the Accel/Gyro chips on the Arbotix-pro?

    There are several options out there, like the Sparkfun Razor, which I had on my Hexapod (may go back on the MK3).
    Likewise PJRC is coming out with a new Prop Shield which is currently in Beta for the Teensy, that has these types of chips on board, or like my Teensy board currently has on it the BNO055. I can easily imagine that if Trossen comes out with a V2 of the Pro, they will also want to enhance this portion of the board.

    I am trying to decide best way on my own board, what levels of information I wish to expose through logical registers, so was wondering if anyone has played around updating the motion code, to see what things could be updated (hopefully improved), if the sensor data was already fused for it...

    Not sure if this makes sense?

    Thanks
    Kurt

  2. #2
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    35

    Re: IMU support - Next gen Arbotiix Pro/ or Playing with my Teensy version of Arbotix-pro...

    I've been using the raw data from the Arbotix-Pro on the HR-OS5 for the localization package in ROS. So far it's been working well enough but I've mainly used it in static conditions for determining the torso angle and connected joints. When there is a lot of noise, like during locomotion, the readings do not appear as accurate as I would like.

    Having an improved inertial sensor that performs the fusion and filtering while providing accurate readings would likely be a nice improvement when I get back into mapping and navigation. Some of my better 3D maps were derived without inertial measurements and strictly relied on visual odometry.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Arbotix Pro ROS support
    By calmur in forum ROS - Robot Operating System
    Replies: 21
    Last Post: 11-05-2019, 04:45 AM
  2. YATB - Yet Another Teensy Board :D
    By KurtEck in forum Arbotix, Microcontrollers, Arduino
    Replies: 126
    Last Post: 12-08-2017, 08:29 AM
  3. PhantomX using a Teensy 3.1
    By KurtEck in forum Humanoids, Walkers & Crawlers
    Replies: 301
    Last Post: 11-17-2016, 01:08 AM
  4. Replies: 7
    Last Post: 01-10-2016, 03:14 AM
  5. Quick question on Arbotix Commander Version 2 - if anyone else had any issues
    By cdraptor in forum Humanoids, Walkers & Crawlers
    Replies: 8
    Last Post: 08-01-2013, 10:16 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •