Results 1 to 7 of 7

Thread: Owners of a PulsedLight LIDAR-Lite v2 Laser Rangefinder click here. Will purchase at high price

Threaded View

Previous Post Previous Post   Next Post Next Post
  1. Owners of a PulsedLight LIDAR-Lite v2 Laser Rangefinder click here. Will purchase at high price

    Hello, my name is Chad Morton, and I am a student at Indiana University studying mathematics and computer programming. For the past year I have been working on a project that uses a LIDAR-Lite Laser Rangefinder v1 by PulsedLight to build point clouds. Nothing new, but my research aims to create, compare, and identify new efficient scanning algorithms, other than the commonly used brute force approach. I recently was invited to present my research at the Butler University Undergraduate Research Conference, which takes place on April 8th. All along I planned to upgrade to the LIDAR-Lite v2, which can take 500 pts/sec, vs the v1, which takes about 50 pts/sec. Until recently had been working on building a software platform and perfecting the physical scanning system. When it finally came
    time to upgrade the LiDAR device, I realized that the v2, which I planned to implement and designed everything around, is on backorder until late April. If I had no other choice, I *could* present with the single v1 I am currently using for testing, however if I had two of the LiDAR v2s, which my rig is set up to run, it would increase the efficiency by 2000%
    (currently running 50 points/sec vs the upgraded 1000 points/sec of two v2s)

    Could anyone help me out here? I would be happy to pay full market price for any used LIDAR-Lite v2s, or even if you could 'rent' me a v2, which I could return to you after my presentation. If you own a LIDAR-Lite v2, PLEASE e-mail me at [email protected] and we can work something out. It would really be a disappointment to have to do my presentation knowing that I am running at only 5% of full potential.

    Here is a video of the rig operating with the v1.
    https://youtu.be/71gEiX26wi4
    and a scan
    http://cs.iusb.edu/~chmorton/output.gif
    Last edited by Squid737; 03-20-2016 at 07:57 PM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Just For Fun LIDAR-lite 360 Mirror Scanner
    By r3n33 in forum Project Showcase
    Replies: 76
    Last Post: 03-20-2016, 12:46 PM
  2. Question(s) Lidar Lite Help to get the distance from the velocity registers
    By cybernetx in forum Sensors
    Replies: 0
    Last Post: 10-05-2015, 03:45 PM
  3. Question(s) Serial Transmission being interrupted by Serial Receiver [Arbotix + Dynamixel AX-12 + LIDAR Lite]
    By rishflab in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 04-14-2015, 05:05 PM
  4. Neato LIDAR Laser Pulse Measurements
    By hash79 in forum Sensors
    Replies: 0
    Last Post: 11-20-2011, 11:41 PM
  5. Question(s) laser eye safety for a scanning laser rangefinder
    By gallamine in forum Robotics General Discussion
    Replies: 23
    Last Post: 11-09-2010, 10:31 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •