Hi!
New to the forums (and robotics), so forgive me 
When trying to run , I'm getting the following error message on my Raspberry Pi (after enabling :
Code:
[Dynamixel Monitor for DARwIn v1.00]
/dev/ttyUSB0 open success!
Set 1000000.0bps success!
TX: FF FF C8 04 03 18 01 17 INST: WRITE
RX: Time:5.10ms RETURN: RX_TIMEOUT
Fail to change Dynamixel power!
Failed to connect Arbotix Pro!
Terminated DXL Manager.
I have tried a different GPIO connector, but no luck. I did accidentally leave the ArbotixPro controller (along with the Raspberry Pi) plugged in all night a couple days ago, if that could have any effect.
It seems that others have solved the problem by either installing a different distro or using the Edison instead, but I wouldn't want to deviate from the recommended configuration unless I have to.
Thanks so much!
Bookmarks