Page 2 of 4 FirstFirst 1234 LastLast
Results 11 to 20 of 31

Thread: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

  1. #11

    Re: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

    As I mentioned, this is not a new issue. There have been a few threads on it, including: http://forums.trossenrobotics.com/sh...to-Arbotix-Pro

    As for using other boards, It all depends. For example suppose you wish to experiment with RPI3 talking to USB2AX. You simply need to provide 5v to the RPI and it will power the USB2AX through the USB.

    I have used different ones including: https://www.amazon.com/Castle-Creati.../dp/B000MXAR12

    I have also built my own RPI shields which I have used to emulate part or all of the Arbotix Pro, which have their own DC to DC converter that I used to power the RPI through the expansion connector.

    Earlier when I was still doing stuff with the HROS1 and Arbotix Pro. I was also experimenting with having the Arbotix Pro be able to talk using second serial port on Arbotix Pro where I then connected it up to the Hardware Serial port that is part of the expansion connector. (Actually I was probably doing it using Odroid). This requires the usage of a hardware Programmer and an adapter to make this work.

    Hopefully some of the other members have some other ideas. I am also not sure if others like @r3n33 has done much with the HROS1 using RPI or has done most of her work using the Edison?

    Edit: Forgot to mention. I believe there was another user who had some better luck on the RPI by using a different image on it (don't remember if it was Debian or Ubuntu or ...), but it had a Real time Kernel enabled on it....
    Last edited by KurtEck; 08-02-2017 at 10:04 AM.

  2. Re: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

    I don't have problems with the pi, my problems happen on both the pi and edison. All the described errors have been reproduced with both boards.

    I read the other threads, I also noticed a weird formula for calculating the timeout and played around with the values but still no luck.
    I also tried your version of the hros1 framework and had the same result. The tcdrain on the timeout was already merged to their code.

    So basically nothing changed in the last few days, still impossible to use that controller in any way. The only sensible solution I see is to use another controller (reinventing the wheel in the process)..

  3. Re: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

    Should I maybe try to reinstall the firmware on the arbotix pro?

  4. #14

    Re: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

    If it were me, I think I would contact their product support: [email protected]

    It is possible they sent you a second bad board. I would probably try to get them to send you another board and if possible see if they can verify they can talk to the board with a pi and/or Edison.

    Also I was frustrated enough with some similar issues with PI, that I started hacking on the Arbotix Pro code to allow me to bypass the USB (FTDI chip) and talk directly to another UART on the board. My version of the code is up at: https://github.com/KurtE/ArbotixPro/...usart2-talk-pc But the last time I touched it was in Feb of 2016, so I don't remember all the details, like which pins worked. But that might be up on some thread up here.

    Also as Trossen did not put any form of boot loader on the board, you need to program it using a programmer. Looks like they have these in stock, http://www.trossenrobotics.com/pro-programming-kit. I purchased mine before they offered them and I think I purchased it from Digikey (2 parts, the programmer and the adapter board)

  5. Re: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

    If they managed to send me two consecutive bad boards, maybe this platform isn't very stable and doesn't fill me with confidence in the long term
    Also they were cheap enough to send me the replacement board by US mail, which took 3 weeks

  6. Re: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

    Just had my replacement board delivered and will test over the weekend. I had exactly the same symptoms with the first board:

    /dev/ttyUSB0 open success!
    Set 1000000.0bps success!

    TX: FF FF C8 04 03 18 01 17 INST: WRITE
    RX: Time:5.10ms RETURN: RX_TIMEOUT
    Fail to change Dynamixel power!
    Failed to connect Arbotix Pro!

    will let you know if it works with the new board.

  7. Re: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

    So the weekend is over, did it work?

  8. Re: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

    no. Same error. Also tried downloading the dxl monitor code from robotis on my laptop. It doesn't see any ids on the dynamixel bus - not even id 200 for the controller. I have gone back to Trossen support to ask them whether they are able to make this work on any of their boards. No reply as yet.

  9. Re: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

    Yes, Trossen didn't bother to reply to me either. It's been 4 days..

  10. Re: RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi

    I'm in touch with their support now. They have acknowledged the issue and are now actively looking at this. All boards seem to be affected. I think its a firmware issue. I'm cautiously optimistic that we're now moving in the right direction.

Thread Information

Users Browsing this Thread

There are currently 3 users browsing this thread. (0 members and 3 guests)

Similar Threads

  1. Dynamixel error - no torque + red light blinking
    By panthallion in forum HR-OS1 Development and Discussion
    Replies: 16
    Last Post: 05-01-2015, 07:16 AM
  2. Question(s) How to clear Dynamixel Overload error
    By Elmue in forum Robotics General Discussion
    Replies: 20
    Last Post: 02-04-2015, 01:44 PM
  3. Raspberry PI 2 vs. Odroid XU3 to use with Dynamixel SDK and usb2ax
    By Snoopy in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 02-03-2015, 07:19 PM
  4. Question(s) Dynamixel comm_rxtimeout error for linux
    By arman in forum DYNAMIXEL & Robot Actuators
    Replies: 8
    Last Post: 05-21-2014, 07:29 PM
  5. Dynamixel SDK linux: COMM_RXTIMEOUT error
    By Deimos in forum Software and Programming
    Replies: 8
    Last Post: 01-16-2014, 01:38 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •