Originally Posted by
jwatte
Trossen does not have a factory in-house. They, like most other people who sell electronics, contract the manufacture of their electronics boards to electronics manufacturers (colloquially called "board stuffers.")
From the board stuffers, you will typically actually get a fully assembled and sealed box -- board + static bag + collateral/inserts + box + sealing.
If they were to test each board, they'd have to open each box, break the seals, open the anti-static bags, and then test the boards.
But, that's something they already paid the board stuffers/factory to do! Part of the manufacturing plan is a testing plan.
From what I know of that business, it's likely the factory somehow failed to run the proper quality controls, and Trossen was left with a bad batch. While they may sample a board or two out of a batch (opening them, meaning they can't then be sold as "new") that could easily miss a defect rate of 10, or 20, or even 50%.
Bookmarks