Results 1 to 3 of 3

Thread: OpenCM IDE (Ubuntu 14.04)

  1. OpenCM IDE (Ubuntu 14.04)

    Hi guys, I have an opencm9.03 board and I am trying to get it to work on Ubuntu14.04. I can see on their page that the last tested version was 12.04 but I that is not a choice for me. I was able to get the board to work on Windows10 and OSXElCapitan and also Ubuntu12.04. I have followed every guide there is and every fix I've seen. The board is recognized and all but when I upload code to the board, I get a "board is not responding" error. Please, any help that can be offered will be highly appreciated.

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    278

    Re: OpenCM IDE (Ubuntu 14.04)

    Ubuntu 14.04, or Ubuntu 14.04 instance via vmware? Because the USB port of the OpenCM-9.04 is the native port of the STM32, it will reset/disappear with the STM32 during the reset+upload process. This means there is a lag between the board being reset and the board reappearing as a new device on the USB port. I'm not sure how vmware handles new USB devices, but the lag in reappearing might be enough to cause a timeout error in the IDE.

    It might be worth trying to force the OpenCM-9.04 into bootloader mode prior to attempting the upload. Not entirely sure anymore, but it used to be that you had to pull D2 (Port A, Pin 0) high with a resistor to force the bootloader to stay active instead of running the existing code on the STM32. It should work with the OpenCM IDE, but if it does not then the uploader python script I made a while back should also work (have to grab the compiled .bin file from arduino folder in /tmp).
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. Re: OpenCM IDE (Ubuntu 14.04)

    Thanks a lot! That worked(python script). I'm really grateful.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) AX-12A + OpenCM + Monkey programmer = Servo not responding
    By OpenRobot in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 12-04-2015, 09:37 AM
  2. Project OpenCM 9.04 - B and 18 Dynamixel AX-12A servos
    By OpenRobot in forum Power
    Replies: 2
    Last Post: 11-29-2015, 05:23 PM
  3. Darwin Mini / OpenCM 9.04 power-on trouble
    By jwatte in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 07-26-2015, 11:16 PM
  4. Question(s) Control AX/RX Dynamixel with Roboplus task with OpenCM9.04 type C + OpenCM 485 EXP
    By kongguan in forum DYNAMIXEL & Robot Actuators
    Replies: 0
    Last Post: 04-22-2015, 04:21 AM
  5. (Questions) How to use USB2Dynamixel under 64v bit Ubuntu 12.04
    By zhenli in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 02-01-2013, 03:31 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •