Page 1 of 2 12 LastLast
Results 1 to 10 of 19

Thread: Z-363 Spectre 3D Printed Body for Bioloid Premium

  1. #1

    Cool Z-363 Spectre 3D Printed Body for Bioloid Premium

    Hey everyone, figured I should finally share this project with you all. It has been in development on and off for about 1,5 year now. I got the idea while working on my previous project, the Tachikoma. In essence it is using an existing robotics kit and replacing the generic frame parts with extremely awesome looking bits. I was very lucky to pick up a cheap second hand Bioloid Premium and then the tinkering commenced. A quick overview with 3 images: sketch, 3D design, physical reality:

    Click image for larger version. 

Name:	Sketch.png 
Views:	335 
Size:	135.2 KB 
ID:	6554 Click image for larger version. 

Name:	Perspective.png 
Views:	317 
Size:	329.3 KB 
ID:	6555 Click image for larger version. 

Name:	20160409-Small.jpg 
Views:	288 
Size:	101.0 KB 
ID:	6557

    Some specs:
    - It takes 140 hours to print, at layer height 0.2 and 0.25 mm for small and large parts respectively.
    - It consists of 56 separately printed parts.
    - All the Bioloid Premium parts can be dropped in and connected (AX-12A, CM, battery etc).
    - Some range of motion has been sacrificed for cosmetic purposes.

    I'm looking in to doing something commercial with it, in combination with Open Hardware, making all the .stl and or the 3D engineering files available. Additionally I also want to improve the wiring with custom wire shielding by ordering some sleeving from moddiy.com.

    Some WIP images from various stages:

    Click image for larger version. 

Name:	Spectre-0020.jpg 
Views:	277 
Size:	65.4 KB 
ID:	6558Click image for larger version. 

Name:	Spectre-0030.jpg 
Views:	247 
Size:	48.5 KB 
ID:	6559Click image for larger version. 

Name:	20150208_102102.jpg 
Views:	239 
Size:	256.2 KB 
ID:	6560Click image for larger version. 

Name:	many-parts.jpg 
Views:	254 
Size:	227.2 KB 
ID:	6562Click image for larger version. 

Name:	Spectre.jpg 
Views:	235 
Size:	106.2 KB 
ID:	6564Click image for larger version. 

Name:	spectre-w-cannon.png 
Views:	256 
Size:	437.7 KB 
ID:	6565Click image for larger version. 

Name:	20150306-smaller.jpg 
Views:	231 
Size:	90.6 KB 
ID:	6566Click image for larger version. 

Name:	20160115-smaller 2.jpg 
Views:	249 
Size:	126.3 KB 
ID:	6567Click image for larger version. 

Name:	20160115-smaller.jpg 
Views:	243 
Size:	125.8 KB 
ID:	6568
    Last edited by CasperH; 04-22-2016 at 04:25 AM.

  2. #2

    Re: Z-363 Spectre 3D Printed Body for Bioloid Premium

    That looks awesome! The final thing looks a lot like the 3D model, too, which is a great sign :-)

    Did you verify mobility ranges and wiring in the 3D model before printing?

  3. #3

    Re: Z-363 Spectre 3D Printed Body for Bioloid Premium

    That looks awesome!
    Thank you!

    The final thing looks a lot like the 3D model, too, which is a great sign :-)
    I sure hope so, something would be very wrong indeed! 3D printing has a tolerance of about -/+ 0.15 mm in the X and Y directions so that is something to keep in mind when making parts that have to fit together.

    Did you verify mobility ranges
    Yes, I verified them during the design using joint assemblies in 3D. However, as mentioned I did have to sacrifice some range of motion for the looks of the robot. The generic bioloid parts have more range of motion, but not all of it is really needed in my opinion.

    and wiring in the 3D model before printing?
    Where possible I compared with a still partly assembled Bioloid Premium model on how the wires go. The thing that proved challenging and which I am still working on is the torso area where everything comes together with the controller. For improved integration I plan on making cables to custom lenghts and running them through the 3D printed parts. This will clean up the model and will make sure no wires snag on to something during movement.

  4. #4

    Re: Z-363 Spectre 3D Printed Body for Bioloid Premium

    Sounds like a good approach.
    What software are you using?

  5. #5

    Re: Z-363 Spectre 3D Printed Body for Bioloid Premium

    Since the end of the Tachikoma project I am running with Fusion 360. It's a new piece of software from Autodesk. The reason it is called Fusion is because it allows for both shape like parametric modelling and the more straight forward solid modelling. It's free for hobbyist and small businesses. Aside from the modelling features is also has integrated CAD/CAM CNC tooling and integration with 3D print utilities. For teamwork it allows project invites and it has a sort of Git like system for version control. I really like it.

  6. #6
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    14

    Re: Z-363 Spectre 3D Printed Body for Bioloid Premium

    Dude that looks great. Like a Gundam.

  7. #7
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    32

    Re: Z-363 Spectre 3D Printed Body for Bioloid Premium

    I really like those models! I think it would be great to see some of those parts illuminated
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  8. #8
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    14

    Re: Z-363 Spectre 3D Printed Body for Bioloid Premium

    Any updates on this? Would be cool to see it in action.

  9. #9

    Re: Z-363 Spectre 3D Printed Body for Bioloid Premium

    Quote Originally Posted by _ADAM_ View Post
    Any updates on this? Would be cool to see it in action.
    Thanks Adam.

    I pretty much finished printing all the parts, but I ran out of M2 bolts during assembly. They should arrive any day now. Once I have that, it will be standing up on it's own. No movements/software routines yet though.

  10. #10

    Re: Z-363 Spectre 3D Printed Body for Bioloid Premium

    Annnnddd... done. For now anyway.

    Click image for larger version. 

Name:	20160620_221326.jpg 
Views:	292 
Size:	83.8 KB 
ID:	6611 Click image for larger version. 

Name:	20160620_221352.jpg 
Views:	273 
Size:	81.6 KB 
ID:	6612 Click image for larger version. 

Name:	20160620_221406.jpg 
Views:	339 
Size:	73.3 KB 
ID:	6613

    Click image for larger version. 

Name:	20160620_221521.jpg 
Views:	258 
Size:	79.9 KB 
ID:	6614

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Bioloid Premium issues (HELP)
    By tbates03 in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 07-30-2014, 08:22 PM
  2. Spectre - 3D printed android Hexapod
    By WGhost9 in forum Project Showcase
    Replies: 16
    Last Post: 03-08-2013, 05:37 AM
  3. Premium Bioloid Kit with AX-S1
    By Hellfire in forum Robotics General Discussion
    Replies: 1
    Last Post: 02-27-2012, 10:12 PM
  4. WTB - Bioloid Premium
    By xnonox in forum Garage Sale
    Replies: 3
    Last Post: 12-27-2011, 11:22 PM
  5. Bioloid Premium Kit
    By cdraptor in forum Robotics General Discussion
    Replies: 3
    Last Post: 08-05-2009, 11:26 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •