Results 1 to 5 of 5

Thread: Dynamixel MX-106T with arduino feedback problems

  1. #1
    mtete Guest

    Dynamixel MX-106T with arduino feedback problems

    Hello,

    I wired a Dynamixel MX-106T with a Arduino Uno just like on this website:
    http://savageelectronics.blogspot.nl...xel-ax-12.html

    And here is the wire schem:
    http://3.bp.blogspot.com/-PhiRUiPEdn...1600/g4084.png

    And this library:
    https://github.com/zcshiner/Dynamixel_Serial

    It works half, I can make the set the Dynamixel in wheel or servo mode.
    But I cannot get any feedback from the Dynamixel.

    ################################################## #####
    Servo ID:1 NO! packet recived from Dynamixel
    Servo ID:1 NO! packet recived from Dynamixel
    Servo ID:1 NO! packet recived from Dynamixel
    Servo ID:1 NO! packet recived from Dynamixel
    Servo ID:1 NO! packet recived from Dynamixel
    ################################################## #####


    De half to full duplex I use:
    http://nl.farnell.com/texas-instrume...ver/dp/1607639

    I cannot find a solution, googled the heck out of it.
    Tried different arduino uno's and a Mega.
    Applied 12V, wired the thing over about 10 times.

    I also tried different Library's but they did not work at all.

    Do somebody knows a solution?

    Thank you.
    M.

  2. #2

    Re: Dynamixel MX-106T with arduino feedback problems

    First, make sure that the servo works OK and is not damaged. Use an USB2AX or USB2Dynamixel to do this, with the Dynamixel Wizard program from Robotis.

    Once that's done, you can try different things. Most important is to figure out whether the problem is that you're holding the wire high when you shouldn't, or whether you're not properly receiving the data but the data is actually on the wire.
    Easiest might be to wire TX to a 1 kOhm resistor, then that resistor to the TTL bus and to the RX pin of your Arduino.
    That way, you will receive everything you send, which you have to manually read and discard. But, then, anything the servo sends should also be received by the RX.
    It's not a super efficient way of doing bi-directional -- servos will drain about 5 mA when sending -- but it will get the job done.

    It also helps if you have an oscilloscope, and/or a logic analyzer.

  3. #3

    Re: Dynamixel MX-106T with arduino feedback problems

    Would help to see your actual code and picture of your actual hookup.

    I have a board that uses the SNLS241, like you mentioned here, however I am using it with a Teensy 3.2 processor. I am also using my own library code, which I adapted to optionally use a direction pin.

    However my changes to my library currently would not work unchanged with the Arduino UNO. As it relies on support that Teensy has built in to the hardware serial port code to automatically change the direction port when the outputs have completed. Where on the UNO you would need to do the changes to the direction pin manually using digitalWrite.

    From your description I assume you have an IO pin connected up to pins 1 and 19 of the SNLS241. Likewise I assume your program calls off to Dynamixel.setDirectionPin with that IO pin. There are some minor things I would play with in the library you are mentioning to see if it makes a difference. Like in DynamixelClass::transmitInstructionPacket not sure why they are disabling interrupts during trying to send the end of the packet. I would have a tendency to comment out the noInterrupts() and interrupts() calls. I would also probably simplify and always call: _serial->flush();

    And as jwatte mentioned, I would also hook up a Logic Analyzer to see what data is being sent and likewise see the state of the direction pin.

    Kurt

  4. #4

    Re: Dynamixel MX-106T with arduino feedback problems

    not sure why they are disabling interrupts during trying to send the end of the packet
    My guess is to get a precise end of the packet, to know when to flip the I/O pin, so it doesn't hold the bus too long?
    I haven't read the code, so if I/O pin flipping isn't inside the interrupt bracket, then that's not it.

  5. #5

    Re: Dynamixel MX-106T with arduino feedback problems

    Quote Originally Posted by jwatte View Post
    My guess is to get a precise end of the packet, to know when to flip the I/O pin, so it doesn't hold the bus too long?
    I haven't read the code, so if I/O pin flipping isn't inside the interrupt bracket, then that's not it.
    Possibly, but if your hardware Serial port works on ISR to queue bytes, may never complete...
    The function, that makes me nervous...
    Code:
    void DynamixelClass::transmitInstructionPacket(void){                                   // Transmit instruction packet to Dynamixel
    
        if (Direction_Pin > -1){
            digitalWrite(Direction_Pin,HIGH);                                               // Set TX Buffer pin to HIGH
        }
    
        _serial->write(HEADER);                                                             // 1 Write Header (0xFF) data 1 to serial
        _serial->write(HEADER);                                                             // 2 Write Header (0xFF) data 2 to serial
        _serial->write(Instruction_Packet_Array[0]);                                        // 3 Write Dynamixal ID to serial
        _serial->write(Instruction_Packet_Array[1]);                                        // 4 Write packet length to serial
        _serial->write(Instruction_Packet_Array[2]);                                        // 5 Write instruction type to serial
    
        unsigned int checksum_packet = Instruction_Packet_Array[0] + Instruction_Packet_Array[1] + Instruction_Packet_Array[2];
    
        for (unsigned char i = 3; i <= Instruction_Packet_Array[1]; i++){
            _serial->write(Instruction_Packet_Array[i]);                                    // Write Instuction & Parameters (if there are any) to serial
            checksum_packet += Instruction_Packet_Array[i];
        }
    
        noInterrupts();
    
        _serial->write(~checksum_packet & 0xFF);                                            // Write low bit of checksum to serial
    
    #if defined(__AVR_ATmega32U4__) || defined(__MK20DX128__) || defined(__AVR_ATmega2560__) // Leonardo and Mega use Serial1
        if ((UCSR1A & B01100000) != B01100000){                                             // Wait for TX data to be sent
            _serial->flush();
        }
    
    #elif defined(__SAM3X8E__)
    
        //if(USART_GetFlagStatus(USART1, USART_FLAG_TC) != RESET)
            _serial->flush();
        //}
    
    #else
        if ((UCSR0A & B01100000) != B01100000){                                             // Wait for TX data to be sent
            _serial->flush();
        }
    
    #endif
    
        if (Direction_Pin > -1){
            digitalWrite(Direction_Pin,LOW);                                                //Set TX Buffer pin to LOW after data has been sent
        }
    
        interrupts();
    
    }
    Again I may be wrong, but personally I would try to simplify some, like:
    Code:
    void DynamixelClass::transmitInstructionPacket(void){                                    // Transmit instruction packet to Dynamixel
    
        if (Direction_Pin > -1){
            digitalWrite(Direction_Pin,HIGH);                                               // Set TX Buffer pin to HIGH
        }
    
        _serial->write(HEADER);                                                              // 1 Write Header (0xFF) data 1 to serial
        _serial->write(HEADER);                                                              // 2 Write Header (0xFF) data 2 to serial
        _serial->write(Instruction_Packet_Array[0]);                                        // 3 Write Dynamixal ID to serial
        _serial->write(Instruction_Packet_Array[1]);                                        // 4 Write packet length to serial
        _serial->write(Instruction_Packet_Array[2]);                                        // 5 Write instruction type to serial
    
        unsigned int checksum_packet = Instruction_Packet_Array[0] + Instruction_Packet_Array[1] + Instruction_Packet_Array[2];
    
        for (unsigned char i = 3; i <= Instruction_Packet_Array[1]; i++){
            _serial->write(Instruction_Packet_Array[i]);                                     // Write Instuction & Parameters (if there are  any) to serial
            checksum_packet += Instruction_Packet_Array[i];
        }
    
        _serial->write(~checksum_packet & 0xFF);                                             // Write low bit of checksum to serial
    
        _serial->flush();
        if (Direction_Pin > -1){
            digitalWrite(Direction_Pin,LOW);                                                 //Set TX Buffer pin to LOW after data has been sent
        }
    
    }
    Or better yet use a Teensy!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Dynamixel torque control using current feedback
    By Gray Fox in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 11-22-2017, 02:04 AM
  2. Question(s) Dynamixel MX-64T current feedback
    By LuPalm in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 01-23-2013, 11:20 PM
  3. Question(s) Regarding Dynamixel Positional Feedback Demo
    By DiegoSpinola in forum Robotics General Discussion
    Replies: 4
    Last Post: 12-06-2011, 05:09 PM
  4. Upload problems with Arduino Duemilanove!
    By cross1933 in forum Software and Programming
    Replies: 8
    Last Post: 05-22-2009, 12:37 PM
  5. Question(s) Arduino serial problems
    By ROBOTMAN in forum Arbotix, Microcontrollers, Arduino
    Replies: 10
    Last Post: 05-09-2009, 10:59 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •