Results 1 to 3 of 3

Thread: Darwin-Mini project with OpenCM IDE

  1. Darwin-Mini project with OpenCM IDE

    A while back I did some work on my Darwin-mini bot using the OpenCM IDE and the ArbotiX Pose Engine.
    It's been a while since I worked on it, but the code could be useful to anyone else looking to replicate the motions and actions.
    You can find the code here

    Features/Solved problems:
    • Python script that converts the ROBOTIS software v2.0 gaits to Bioloid motion controller gaits (needs some manual touch ups once generated). File is called mtn2cm9rpm.py
    • On the fly motion adjustments for speed
    • IMU_MPU6050 integration for gyro and accelerometer readings over i2c
      • auto get up function when robot falls over

    • Servo performance problem when using XL-320 with OpenCM
    • Motions have been exported from ROBOTIS controller to Bioloid motion controller including:
      • Get Up
      • Sit
      • Greet 1
      • Greet 2
      • Right/Left Hook
      • Right/Left Kick
      • Right/Left Turn
      • Side Step Left/Right
      • Advance
      • Fast Advance
      • Slow Advance
      • Reverse


    Unsolved problems:
    • robot shakes after programming if battery power is on
    • if robot falls over hard it can result in the robot shaking and all servos flashing red
    • programming space limited to about half the full amount due to a firmware bug by ROBOTIS (non of the fixes worked for me)
    • i2c magnetometer integration



    This is by no means finished code, it is very much a work in progress. It will require some stuffing around to get it working as I haven't worked on this project in a while.
    Last edited by klims; 05-01-2016 at 08:12 AM.

  2. #2

    Re: Darwin-Mini project with OpenCM IDE

    That sounds great! I have a Darwin Mini, too, that I sometimes poke at.

    The main problem for me is that it's "use the stock software" or "start from scratch," and while I'm capable of starting from scratch, that's a giant time suck.

    What I really just want to do is add support for firing a laser while controlling the robot walking around (demo purposes!) so I'm considering re-purposing a Onyx Fire II board to read DXL 2 commands, and just configure it to turn on when the "position" is > 800 or something. The main problem that drives that is that the Robo+ software doesn't support peripherals, only the XL-320 motors (and the upcoming other X ones.)

  3. Re: Darwin-Mini project with OpenCM IDE

    Yeah feel free to grab it as a code base and add on to it

    I forgot to mention that you will either need to send the bot commands via USB or a bluetooth serial link.
    I used an app I wrote a while back to push characters over bluetooth serial from my android device. You can find it here
    I have a new version I have written that works on multiple device resolutions and is much nicer to use, but I don't have anywhere to host the APK.
    PM me if you want to check it out

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Darwin Mini, R+ Motion 2.0, how to add switched objects?
    By jwatte in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 05-02-2016, 10:59 AM
  2. SDF for for Bioloid or Darwin Mini?
    By jwatte in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 08-22-2015, 04:03 PM
  3. Darwin Mini / OpenCM 9.04 power-on trouble
    By jwatte in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 07-27-2015, 12:16 AM
  4. Question(s) Darwin Mini and RoboPlus Task
    By Det in forum Software and Programming
    Replies: 17
    Last Post: 05-03-2015, 05:48 AM
  5. HELP - Darwin Mini
    By PhilMonty in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 08-02-2014, 08:52 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •