Page 4 of 4 FirstFirst 1234
Results 31 to 34 of 34

Thread: UP Board

  1. #31

    Re: UP Board

    Again I don't have schematic, but was told they do have at least a poly-fuse and then voltage regulator...

    I did try applying 5v to RPI like header pins and the 3.3v pins show correctly so some of it is still working. But not sure what else.
    Does not appear to boot up to the WIFI... Not sure I wish to plug it into HDMI to see if anything shows up... But may with monitor I don't care if I fry...

  2. #32

    Re: UP Board

    ... I did try with monitor that I don't care about and nothing (as I suspected would happen).

    It was sort of interesting yesterday, that when I made the order for the replacement plus a few extras.

    When I completed the order, at the end of my order it took me to a page showing what turned out to be a test for a flash sale, which if it was real I would probably have ordered...

    Realsense R200 with UP board, cable and power supply for $120)... So I contacted them...

    Turned out it was just a test and not a real product code or I would have been able to add it to order... Note they do sell the higher end Realsense camera: http://up-shop.org/home/117-up-zr300...ement-kit.html

    In one of my replies to them, I mentioned that I thought it would be a nice product as currently the Turtlebot-3 waffle shows this camera with Intel Joule, which we know is in the process of being discontinued.

    I received a response from them of: Very soon you will hear some update about UP and Turtlebot3. :-)

    And later this morning they send out email to their list announcing a Summer Flash sale starting at midnight tonight (not sure whose midnight). http://up-shop.org/

    So who knows what they will have up there.

  3. #33

    Re: UP Board

    Aluminum chassis + up2 might make for a good home theater PC. Or perhaps a 3D printer runner. (I have a little AMD-based Z-box from many years ago that initially went on the first Onyx walker doing that duty right now. It's very slow.)
    Then again, at $200-$300, there are NUCs with similar capability and price, available from Amazon ... like http://amzn.to/2tjOIKv
    You'd need to use USB for the Teensy, though; no RPi header.
    Last edited by jwatte; 07-20-2017 at 02:52 PM.

  4. #34

    Re: UP Board

    My UP2 board arrived. First thing that hit me, is how much more bulky this board is versus the first UP board.
    Click image for larger version. 

Name:	Up Boards.JPG 
Views:	68 
Size:	121.6 KB 
ID:	7083

    There is an RPI3 sitting behind the UP2.

    They grew the board in one direction, but the but difference is the size of the Heatsink below the board. It also came with a case, which I had it in, but yesterday I received a Wifi/BT board, like you use in a portable which I installed. Not sure yet about Ant. I purchased a couple of external ones to plug in, but they are rather bulky.

    Now back to playing

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. my ssc-32 board not working ?
    By omercyprus in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 05-05-2012, 09:05 AM
  2. My new Serial Servo Board with on Board RAM :-)
    By Pinter75 in forum Project Showcase
    Replies: 4
    Last Post: 03-03-2010, 10:53 PM
  3. Question(s) Help with Sonar and what I/O Board?
    By nagmier in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 05-21-2009, 08:43 AM
  4. Need suggestions for new board
    By sniperscope in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 05-08-2009, 04:12 PM
  5. relay board
    By TSPCO in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 02-26-2009, 10:49 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •