Results 1 to 2 of 2

Thread: Can Arbotix Pro easily replace the Arbotix-M in my robot?

  1. Can Arbotix Pro easily replace the Arbotix-M in my robot?

    I have an Arbotix-M that I use as a subcontroller for a legged robot. It runs a modified Firmata sketch compiled with Arduino to interface with a realtime controller on my Windows machine.

    I have my eye on the Arbotix Pro, mostly for its additional analog pins and the built in gyro and accelerometer. Aside from geometry, is it a one-to-one replacement? Can I still run my Arduino code on it? Are there major differences between the two? I've had a hard time finding any documentation on them.

    Thanks,

    NSz

  2. #2
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    16

    Re: Can Arbotix Pro easily replace the Arbotix-M in my robot?

    There was recently some discussion in this thread that may help answer your questions:
    http://forums.trossenrobotics.com/sh...-Now-Available!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Biped Robot with Arbotix + Dynamixel AX-12A
    By kanuto in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 11-09-2014, 04:58 PM
  2. URDF, Robot State Publisher, and the ArbotiX
    By Peter_heim in forum ROS - Robot Operating System
    Replies: 9
    Last Post: 04-26-2014, 08:48 PM
  3. Question(s) ArbotiX with LabVIEW: Low-level ArbotiX Commands?
    By vogonpoet42 in forum Software and Programming
    Replies: 2
    Last Post: 03-01-2013, 10:25 AM
  4. Question(s) Adding XBee Wi-Fi & webcam to existing ArbotiX Robocontroller robot
    By Stephen in forum Mechanics / Construction
    Replies: 7
    Last Post: 12-07-2012, 12:20 PM
  5. Arbotix vs. Propeller Robot Control board?
    By Stobs in forum Mech Warfare
    Replies: 9
    Last Post: 12-30-2010, 04:43 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •