First, sorry if I'm using the wrong terminology, hope you understand what I mean.
On the back of the Dynamixels, there is a hole on the same axis as the output shaft that is typically used to mount idlers for "hinge" brackets.
I'm wondering if this mount point is connected to and supports the output shaft that drives the horn. I kind of assume it is but I am not sure, and I don't want to dismantle one. I'd like to know for AX-12, MX-28 and MX-64.
If so, then it will be beneficial to support the output shaft and reduce the lateral load, which is bad for the gears. If not, then it may not be worth the extra work and added weight.
If it is, then it will affect how I will design joints where a hinge bracket is not used, such as humanoid shoulder pitch or hip yaw.
Bookmarks