Page 2 of 2 FirstFirst 12
Results 11 to 15 of 15

Thread: DPDT 3-Position Switch On-Off-Charge Wiring

  1. #11
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    17

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    Hey tician. I'm looking at this one - 30 amp 12VDC DPT 3-Position On-Off-On:

    http://www.gamainc.com/site/epage/130301_941.htm

    My plan is to connect a male/male deans-style on a short wire to each "row" of the DPDT. Then connect one male deans to the battery, one to the charge cable, and one to main output (a Y harness where one goes to a BEC and RPi, other straight to Dynamixel power bus).

    I like this setup because it's clean and modular, can easily take things apart and change them out if I want.

    I want easy acces for charging without disconnecting anything, and I don't want the charge cable on the same circuit as main power. Balance connector will also be easily accessible.

    I understanding everyone looks at this kind of stuff a little differently, and this setup makes sense to me.

  2. #12
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,315
    Images
    27
    Rep Power
    280

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    Should work fine although there may be hiccups/reboots during switching if supplying external power to the BEC and RPi upstream of the battery switch. Definitely verify the terminals of the switch before powering everything up. Center pair should be the 'common' lines and be connected to battery, but the switch drawing does not state that explicitly.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #13
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    17

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    I would not switch it off unless I shutdown linux first, if that's what you mean.

    If you're saying it might not boot cleanly from cold, then that's something I'd need to look at. I'm also looking at maybe using the MoPi power board... not sure though, will prototype without it first.

    There will be a momentary button that executes a shutdown sequence. Or I can do it from putty when I'm at my desk.
    Last edited by _ADAM_; 06-03-2016 at 03:54 PM.

  4. #14

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    You want the connection to the charger and to the bot to be female, just like a battery connector, and you want the connector to the battery to be male, to mate with the battery.
    The reason for this will become obvious once you start playing around with hooking up diferent pieces.
    Specifically, you'll want to be able to plug the battery straight into the bot without the switch, as well as with the switch.
    You also want to be able to plug the charger into the switch, as well as straight into the battery.

  5. #15
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    17

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    Agree J on M/F comments, that's exactly how I have it drawn up (pen and paper, how I design everything).

    Waiting on some parts, but I'll start a bot-specific thread and post pics of everything when it's ready.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Servo reading position and lock position CW
    By mkanon in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 03-30-2013, 05:10 PM
  2. Kill switch?
    By Stobs in forum Mech Warfare
    Replies: 7
    Last Post: 08-06-2010, 12:02 AM
  3. Question(s) exceeded DPDT Switch's rating = very hot battery
    By kfrench in forum Power
    Replies: 16
    Last Post: 12-14-2009, 07:40 PM
  4. Wiring the 0/16/16
    By modularia in forum Arbotix, Microcontrollers, Arduino
    Replies: 14
    Last Post: 09-30-2008, 02:22 PM
  5. Charge multiple power packs
    By Connor in forum Power
    Replies: 9
    Last Post: 08-30-2008, 09:20 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •