Page 1 of 2 12 LastLast
Results 1 to 10 of 15

Thread: DPDT 3-Position Switch On-Off-Charge Wiring

  1. #1
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    22

    DPDT 3-Position Switch On-Off-Charge Wiring

    Hi,

    I want to use a DPDT 3-position switch to do On-Off-Charge wiring. In the diagram below, Main would go to the robot electronics and Charge would go to a dangling female power cable so that the battery could be charged without disconnecting anything. Just flip the switch and charge.

    I'm not an expert on electronics... it would be great if someone can tell me whether this wiring is correct or not. I don't want to smoke something or start a fire!



  2. #2
    Join Date
    May 2016
    Location
    White Plains, NY
    Posts
    124
    Images
    1
    Rep Power
    21

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    There's no need to switch both positive and negative. I would tie the negatives together, separately from the switch, and switch just the +'s. So a single-pole switch would be adequate. If you end up with a double-pole switch, bridge each pole of the switch so the current is shared across the poles of the switch.

    Keep in mind that if you want to use a balance changer you'll want to provide access to the battery's balance connector.

    Also keep in mind that you REALLY don't want to charge the battery while it's in your machine. Firstly you can't see the battery if it develops problems, and secondly if it catches fire it will damage your machine. RC enthusiasts typically remove the battery and charge it while in a ceramic flower pot or something that you can readily pick up and run out the front door with...

  3. #3
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    860
    Images
    25
    Rep Power
    95

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    Quote Originally Posted by Brooks View Post
    Also keep in mind that you REALLY don't want to charge the battery while it's in your machine. Firstly you can't see the battery if it develops problems, and secondly if it catches fire it will damage your machine. RC enthusiasts typically remove the battery and charge it while in a ceramic flower pot or something that you can readily pick up and run out the front door with...
    In the beginning of lipo being used in the hobby I did this religiously. (Especially since not all chargers had a balance connector in the early days.) Now that I'm exclusively in robotics and these batteries don't get knocked around like in quadcopters and cars plus we have voltage reporters out there I tend to leave mine in.

    Quote Originally Posted by Brooks View Post
    Keep in mind that if you want to use a balance changer you'll want to provide access to the battery's balance connector.
    Which I strongly suggest as well. Even the highest quality lipo cells drift in voltage on discharge. (Now that I think about it that could easily cause bad things to happen if you overcharge a cell since another cell could be bad or dead.)

  4. #4
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    22

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    Thanks for the replies. FYI I have more than a decade of experience with lipos in RC and robotics.

    I really wanted to know if my understanding of how the switch works is correct. If I wired it how I have it shown in the diagram, would it work as I expect?

  5. #5
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    860
    Images
    25
    Rep Power
    95

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    Since you are doing something more than a simple Arduino project. Take a look at this. http://www.mini-box.com/OpenUPS I'm integrating it into the Golem MKII project in the next week or so. It might be something you would be interested in.

  6. #6
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    22

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    Thanks. Not sure it fits my project, but I'll add it to my ever-growing list of cool parts to consider.

    Quote Originally Posted by KevinO View Post
    Golem MKII project
    Oooh, that sounds interesting...

  7. #7

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    First: Most DPDT switches are only rated for a few dozen milliamps, not the up to the dozen amps you'll need to pull through the battery wires.

    Second: There's no rule that the bot can't be powered while charging. The way I solve this problem is simply have a "charge input" connector in parallel with the battery. This means that I can power the bot itself from a power supply, and I can charge the battery, and I can run untethered (by disconnecting the wire.) The one danger is if I keep the power at "max charge" voltage for long after the battery is fully charged, I'll reduce the life of the battery.

    Now, this is convenient for other reasons, too. For example, maybe my power supply can only supply a few amps. When paralleled with the battery, the battery will provide more current during times of high draw, yet will stay charged on average because the power supply.
    I tend to "float" the batteries like this at 3.95 Volts per cell, which I believe is low enough to not wear out (really, metalize) the batteries, yet is high enough that the battery has a decent charge when disconnecting. If I need to go unwired for long, I raise the voltage to 4.2V per cell, and wait until the power draw on the power supply is a few dozen milliamps, and then unplug -- this is the CC/CV charge that LiPos are supposed to get to get to top charge. And once in a while, I do a "balance charge" using an actual charger with the balance connector attached.

    So, anyway -- most DPDT switches are not rated for nearly the current you need, which means they might burn up from contact resistance.
    Parallel battery and "charge in" without switch, and you have the most flexibility.

    As I posted in another thread, I then also use a software controlled power switch (power MOSFET) which lets me disconnect the battery when it runs out of juice, to avoid killing it. But that's gravy -- if you use a LiPo Guard "beeper" type device, you'll probably do fine manually.

    you REALLY don't want to charge the battery while it's in your machine
    Yet, laptops, cell phones, and cameras, do this all the time. I mount my batteries with reasonable protection, and I treat them well, and I haven't had a problem with batteries burning up in many years. So, your mileage may vary, and what's good for me may not be good for you, but I think that rule comes from times when hobbyists didn't use the right kind of chargers, and from when batteries would be knocked around in cars and such and thus take damage.
    Last edited by jwatte; 06-02-2016 at 11:45 PM.

  8. #8
    Join Date
    May 2016
    Location
    USA
    Posts
    145
    Images
    12
    Rep Power
    22

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    Thanks for the info. There are heavy duty switches that can handle the current if I decide to go that route. I wouldn't use a wimpy switch.

    I still would like to be sure if I understand how the switch's terminals are connected. Based on my diagram, if the switch is in the "up" direction, the Battery and Charge terminals would be connected, and if the switch is in the "down" direction, the Battery and Main terminals would be connected. Please let me know if that's right or wrong, the schematic is like hieroglyphics.

  9. #9
    Join Date
    May 2016
    Location
    White Plains, NY
    Posts
    124
    Images
    1
    Rep Power
    21

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    The answer to your question is yes. Please keep in mind everyone's comments!

  10. #10
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    284

    Re: DPDT 3-Position Switch On-Off-Charge Wiring

    Do you have a manufacturer name and model number for the switch(es) you are looking at? The image is not exactly informative.

    Probably easier - and maybe safer? - to just have one switch controlling power to the bot and a second connecting the battery/charger to bot power (can keep the bot powered while charging by keeping the external supply connected and flipping only the battery switch to isolate it from the bot). Run the risk of an accidental power-off if forget to flip the battery switch and reconnect the battery when unplugging the external supply.

    I've been working on a far more complicated solution by implementing several components of the standard I2C 'Smart Battery' specifications partly because the battery in my netbook is kaput, but mostly because it would be very nice for swappable robot/moped batteries. A couple arduino libraries for talking to smart batteries with the software I2C library already exist.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 2 users browsing this thread. (0 members and 2 guests)

Similar Threads

  1. Servo reading position and lock position CW
    By mkanon in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 03-30-2013, 04:10 PM
  2. Kill switch?
    By Stobs in forum Mech Warfare
    Replies: 7
    Last Post: 08-05-2010, 11:02 PM
  3. Question(s) exceeded DPDT Switch's rating = very hot battery
    By kfrench in forum Power
    Replies: 16
    Last Post: 12-14-2009, 06:40 PM
  4. Wiring the 0/16/16
    By modularia in forum Arbotix, Microcontrollers, Arduino
    Replies: 14
    Last Post: 09-30-2008, 01:22 PM
  5. Charge multiple power packs
    By Connor in forum Power
    Replies: 9
    Last Post: 08-30-2008, 08:20 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •