Hi everyone,
Welcome to the build thread for my new custom Phoenix-based hexapod project named ALPH (or just Alph)!
The hexapod will use AX-12+ actuators and will be powered by a Raspberry Pi running custom Java code. Gait engine will be a port of "that" code base.
I scored these 18 AX-12+ from a used Comprehensive kit for a good price. They look basically brand new. They have none of the surface scratches you would see on assembled actuators. The two AX-12+ up top are for the "head" and were also scored used in a bundle deal a while back.
Here is a picture of the Phoenix parts, some brackets, and some 0.09" 5052 bar stock. FYI, as of this writing, the Lynxmotion Phoenix chassis kits are on sale for $12 and the femur pairs are on sale for $5! The chassis kit comes with a lot of extra parts such as aluminum standoffs, bearings, hardware, wiring. I'm using some other Lynxmotion parts that will be revealed later.
Here is a picture of the electronics, including Raspberry Pi 3, Samsung 16GB Micro SD, EzConnect HAT, USB2AX, Turnigy 5A UBEC, Turnigy 3000mah lipo, Arbotix power hub, DPDT 30 amp 12VDC switch, momentary switch, Deans Ultra connectors (will use about 8 pairs). Sensors/cameras not shown, TBD. There will also be a Bioloid 6-Port Cable Hub, need to order it. Also working on the wiring, but all the TTL wires will be wrapped as shown in the USB2AX.
Just getting started. As always, your thoughts, opinions, and random robotic musings are welcome.![]()
Bookmarks