Results 1 to 4 of 4

Thread: HR-OS1 shaking when standing

  1. Exclamation HR-OS1 shaking when standing

    My HR-OS1 lurches back and forth when it's standing during ps3_demo. If I pull its torso back slightly, the issue stops (and I can walk), but if I stop walking again the issue often restarts. Unfortunately, I'm having other problems and so can't post a video, but its torso rapidly shakes back and then forward again and again until manually corrected.
    Should I change settings in the walk tuner, tighten screws, ...?
    Thanks for the help!

  2. #2
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    33

    Re: HR-OS1 shaking when standing

    Sounds to me like the balance gain might be just a little too high. I'd definitely check the screws since there is always one or two that find a way of coming loose over time.

    In walk tuner you can try adjusting the "Balance knee gain" and "Balance ankle pitch gain" by -0.01 until the issue is improved.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  3. Re: HR-OS1 shaking when standing

    I could observe the same behavior during the ps3_demo! Did anyone find a solution yet?

    Also I have the problem that I don't know how to stop the demo, since the stop_ps3_demo program does not exist as stated in the tutorial. The only way I can stop it is to turn it off. How do you make it stop?

  4. #4
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    33

    Re: HR-OS1 shaking when standing

    Quote Originally Posted by Alexi View Post
    I could observe the same behavior during the ps3_demo! Did anyone find a solution yet?

    Also I have the problem that I don't know how to stop the demo, since the stop_ps3_demo program does not exist as stated in the tutorial. The only way I can stop it is to turn it off. How do you make it stop?
    Did you try my suggestion? The adjustable parameters in walk_tuner are used in any project using the motion manager and walking module from the framework including ps3_demo.

    You are correct about the stop_ps3_demo script being missing. I'm actually not sure why and don't see that I've ever had a copy in my fork of the OS1 framework. However I believe you can call 'sudo killall demo' or make a script that does this for you to stop the ps3_demo and prevent you from having to turn the robot off.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Dynamixel servo shaking a lot - should I be worried?
    By kevining in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 01-30-2015, 11:42 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •