Results 1 to 2 of 2

Thread: Phantomx Reactor arm behaves differently in simulation and in practice

  1. #1
    simonzzzzz Guest

    Phantomx Reactor arm behaves differently in simulation and in practice

    Hi everyone!

    I've just recently got into Robotics and the first assignment i've received was to play around with the phantomx reactor arm

    Anyway, i've set up the robot arm to work with Moveit. I've also created a python script which lets the robot draw a circle using the ComputeCartesianPath() method from Moveit.
    When i'm running this code on the Rviz simulator it works just fine. The fraction of the plan is 1.0. All is good.
    However, when i run the code on the actual robot, the returned fraction is only 0.48, and the robot only performs parts of the motion.

    What could be the cause of this difference between simulation and reality? I've had my supervisor triple checked the code and made sure it was okay, so that should not have caused the issue.

  2. #2

    Re: Phantomx Reactor arm behaves differently in simulation and in practice

    I'm not familiar with Moveit, can you tell us a little more about your setup? Are you running ROS/pass through firmware on the ArboitX and controlling from the computer, or are you writing custom firmware for the ArbotiX?

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX Reactor, ROS, MoveIt
    By Adam Glass in forum Interbotix Robotic Arms
    Replies: 8
    Last Post: 09-20-2018, 08:54 PM
  2. ROS Port of Commander.ino for PhantomX Reactor Arm
    By ramabrahma in forum ROS - Robot Operating System
    Replies: 1
    Last Post: 07-04-2013, 07:24 PM
  3. Playing with the PhantomX Reactor
    By Xevel in forum Interbotix Robotic Arms
    Replies: 6
    Last Post: 03-16-2013, 06:24 PM
  4. 3D Model of the PhantomX Reactor Arm
    By nckswt in forum Interbotix Robotic Arms
    Replies: 5
    Last Post: 12-31-2012, 04:49 PM
  5. Kurt's PhantomX Reactor Robot Arm
    By KurtEck in forum Interbotix Robotic Arms
    Replies: 11
    Last Post: 12-10-2012, 05:11 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •