Page 1 of 3 123 LastLast
Results 1 to 10 of 26

Thread: My Advanced Realistic Humanoid Robot Project

  1. #1

    My Advanced Realistic Humanoid Robot Project

    The Project Goal

    I'm planning to build an advanced humanoid robot. Think Ex Machina, The Terminator, Data from Star Trek, etc. I decided to avoid teasing by NOT making it a girl. I'd never live that down. If it was a child, I'd be called a pedo. So that leaves male... So just like Data on Star Trek's creator created Data to look just like him, I'm making mine a mirror image of myself! I want the robot to ultimately move like a human, be able to walk, run, jump, do chores, dance, do sports, have conversations realistically, paint, do sculpture, etc. Hope you enjoy following me on my EPIC journey


    About Me

    I'm Gary from Undisclosed, US. I have a background in computer programming as well as a lot of trades (electrical, mechanical, construction, etc). I also am an artist - sculptor, painter. I consider myself an inventor and an innovator. My current inspiration is Elon Musk.


    Robot Features Planned

    I plan to start out sculpting the left arm and hand, rigging them up with servo motors, connecting that up to a pc, and getting it to grasp. From there I will develop the torso, the scull, the legs, the feet, and the other arm. The bot will have silicone skin and look realistic and move realistic. It will have artificial lungs for cooling. It will have spandex ligaments and pulley systems to imitate muscles. It will have sensors to feel if it bumps into things and it will have webcam eyes. It will have a speaker in the mouth to speak with and the mouth will move to lipsync what it is saying. It will have facial expressions. It will have advanced artificial intelligence. It will run on battery and/or power cable depending on the situation.




    https://www.youtube.com/watch?v=mRTtyT2cWaI


    My website: http://www.artbyrobot.com
    Be sure to checkout artbyrobot.com for more, also my youtube channel http://www.youtube.com/c/artbyrobot
    Last edited by artbyrobot; 01-20-2016 at 10:42 AM.

  2. #2

    Re: My Advanced Realistic Humanoid Robot Project

    My website: http://www.artbyrobot.com


    · Robotic Hand Bones Epoxy Drying



  3. #3

    Re: My Advanced Realistic Humanoid Robot Project

    · Robot Hand Starting to Take Shape


  4. #4

    Re: My Advanced Realistic Humanoid Robot Project

    Interesting! How do you plan to actuate all the bits? Are you planning for it to walk on legs?

  5. #5

    Re: My Advanced Realistic Humanoid Robot Project

    Quote Originally Posted by jwatte View Post
    Interesting! How do you plan to actuate all the bits? Are you planning for it to walk on legs?
    I plan to actuate it with servos pulling on string connected at the joints to simulate muscles. The servos will be placed in areas where muscles or organs would normally be. Also, yes, it will walk on legs.

  6. #6

    Re: My Advanced Realistic Humanoid Robot Project

    How much will the full skeleton weigh?
    Have you calculated how much torque/speed you need in the servos for standing/walking?

  7. #7

    Re: My Advanced Realistic Humanoid Robot Project

    The full skeleton will weigh probably under 2lb. I'm using lightweight epoxy hollow bone construction all handmade. I have calculated some estimates of the torque/speed of the servos for standing/walking but experimentation will be the only way to know for sure I think...

  8. #8

    Re: My Advanced Realistic Humanoid Robot Project

    That's unbelievably light! I look forward to seeing the progress of this project.

  9. #9

    exoskeleton mesh progress

    Click image for larger version. 

Name:	exoskeleton mesh of hand method.jpg 
Views:	188 
Size:	237.1 KB 
ID:	6119Click image for larger version. 

Name:	exoskeleton mesh of hand progress.jpg 
Views:	179 
Size:	245.3 KB 
ID:	6120

  10. #10

    Re: My Advanced Realistic Humanoid Robot Project



    Making the arms exoskeleton using double stick tape then upholstery thread then super glue to hold it firm followed by some epoxy.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Giger-OP - An Open Source Research Humanoid Project
    By DresnerRobotics in forum Humanoids, Walkers & Crawlers
    Replies: 9
    Last Post: 06-05-2014, 09:52 PM
  2. Humanoid Project
    By abhishek001 in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 03-02-2014, 10:57 PM
  3. Question(s) University humanoid robot project, need controller suggestions
    By Jayws in forum Arbotix, Microcontrollers, Arduino
    Replies: 10
    Last Post: 05-05-2012, 11:48 PM
  4. Question(s) choosing platform for project (biped, torque control servo, advanced kinematic)
    By sergeyko in forum Robotics General Discussion
    Replies: 7
    Last Post: 05-16-2011, 01:02 AM
  5. Incredibly realistic Hexabot Movement
    By Matt in forum Humanoids, Walkers & Crawlers
    Replies: 16
    Last Post: 08-05-2008, 07:16 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •