Page 2 of 2 FirstFirst 12
Results 11 to 15 of 15

Thread: ArbotiX 1.6 Files / Libraries

  1. #11
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    96

    Re: ArbotiX 1.6 Files / Libraries

    KurtEck,

    Thanks for the heads up. I gave turning off livesafe, to no avail. I haven't gotten to dig much deeper yet, and probably will now. I am relatively sure it is the programmer that is the problem. I will dig deeper in a little bit following the link you posted...Have some things to take care of around the house first.

    I have ordered an FTDI cable in the meantime, and will try working from fresh on my old computer to see if maybe it is something in the way this new machine does things...though the old computer has been reinstalled several times since the last time I did any of this.

    One thing, is there someplace I should look that would give me more information as to what might be going wrong? I feel like the fact that if I just verify and compile things work means that I am close, and whatever is wrong is with the part that actually gets the program out into the board.

    Thanks again for the help, Any further help would be appreciated. I feel like I was on a path and stepped in mud, and just need someone to pull me free so that I can keep going.

    DB

  2. #12

    Re: ArbotiX 1.6 Files / Libraries

    Hi again, if you used the tician boards install and you have the programmer that Trossens sells, than his setup did not add in the definition for the that programmer. Problem is if you used to use that to program the arbotix than it is very likely it does not have the bootloader any more.

    I edited my configuration to add it in. As I mentioned earlier in this thread, I keep meaning to make my own install with this in it.
    But if you go to where your programmer.txt file is, probably at: C:\Users\Che Edoga\AppData\Local\Arduino15\packages\arbotix\har dware\avr\0.0.2\hardware

    And update the programmer.txt to:
    Code:
    avrispmkiis.name=AVRISP mkII (serial)
    avrispmkiis.communication=serial
    avrispmkiis.protocol=stk500v2
    avrispmkiis.program.tool=avrdude
    avrispmkiis.program.extra_params=-P{serial.port}
    
    
    avrisp.name=AVR ISP
    avrisp.communication=serial
    avrisp.protocol=stk500v1
    avrisp.program.protocol=stk500v1
    avrisp.program.tool=avrdude
    avrisp.program.extra_params=-P{serial.port}
    
    avrispmkii.name=AVRISP mkII
    avrispmkii.communication=usb
    avrispmkii.protocol=stk500v2
    avrispmkii.program.protocol=stk500v2
    avrispmkii.program.tool=avrdude
    avrispmkii.program.extra_params=-Pusb
    
    usbtinyisp.name=USBtinyISP
    usbtinyisp.protocol=usbtiny
    usbtinyisp.program.tool=avrdude
    usbtinyisp.program.extra_params=
    
    arduinoisp.name=ArduinoISP
    arduinoisp.protocol=arduinoisp
    arduinoisp.program.tool=avrdude
    arduinoisp.program.extra_params=
    
    arduinoisporg.name=ArduinoISP.org
    arduinoisporg.protocol=arduinoisporg
    arduinoisporg.program.tool=avrdude
    arduinoisporg.program.extra_params=
    
    usbasp.name=USBasp
    usbasp.communication=usb
    usbasp.protocol=usbasp
    usbasp.program.protocol=usbasp
    usbasp.program.tool=avrdude
    usbasp.program.extra_params=-Pusb
    
    parallel.name=Parallel Programmer
    parallel.protocol=dapa
    parallel.force=true
    # parallel.delay=200
    parallel.program.tool=avrdude
    parallel.program.extra_params=-F
    
    arduinoasisp.name=Arduino as ISP
    arduinoasisp.communication=serial
    arduinoasisp.protocol=stk500v1
    arduinoasisp.speed=19200
    arduinoasisp.program.protocol=stk500v1
    arduinoasisp.program.speed=19200
    arduinoasisp.program.tool=avrdude
    arduinoasisp.program.extra_params=-P{serial.port} -b{program.speed}
    
    usbGemma.name=Arduino Gemma
    usbGemma.protocol=arduinogemma
    usbGemma.program.tool=avrdude
    usbGemma.program.extra_params=
    usbGemma.config.path={runtime.platform.path}/bootloaders/gemma/avrdude.conf
    
    # STK500 firmware version v1 and v2 use different serial protocols.
    # Using the 'stk500' protocol tells avrdude to try and autodetect the
    # firmware version. If this leads to problems, we might need to add
    # stk500v1 and stk500v2 entries to allow explicitely selecting the
    # firmware version.
    stk500.name=Atmel STK500 development board
    stk500.communication=serial
    stk500.protocol=stk500
    stk500.program.protocol=stk500
    stk500.program.tool=avrdude
    stk500.program.extra_params=-P{serial.port}
    
    ## Notes about Dangerous Prototypes Bus Pirate as ISP
    ## Bus Pirate V3 need Firmware v5.10 or later
    ## Bus Pirate V4 need Firmware v6.3-r2151 or later
    ## Could happen that BP does not have enough current to power an Arduino board 
    ## through the ICSP connector. In this case disconnect the +Vcc from ICSP connector
    ## and power Arduino board in the normal way.
    buspirate.name=BusPirate as ISP
    buspirate.communication=serial
    buspirate.protocol=buspirate
    buspirate.program.protocol=buspirate
    buspirate.program.tool=avrdude
    buspirate.program.extra_params=-P{serial.port}
    I added in the part at the start (serial). That after you restart Arduino IDE you should be able to choose in the Tools->Programmer menu

  3. #13
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    96

    Re: ArbotiX 1.6 Files / Libraries

    I am infact using the little usb programmer that trossen sells...or sold years ago, maybe still? In anycase, under tools -> programmer AVRISP mkII is selected, but (serial) is not an option or is not available.

    I updated the programmer.txt file, or at least think I did...

    At this point I have probably made enough of a mess of things that I just need to start over and carefully follow the advice above?

    DB

  4. #14
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    96

    Re: ArbotiX 1.6 Files / Libraries

    Ok...I found a programmer.txt file under an arduino folder in the hardware folder. I edited that one also and the AVRISP mkII (Serial) option appeared. I tried selecting it and uploading and got the following error...

    Arduino: 1.6.13 (Windows 10), Board: "Arbotix-M"


    c:\program files (x86)\arduino-1.6.13\hardware\tools\avr\bin\../lib/gcc/avr/4.9.2/../../../../avr/bin/ar.exe: unable to rename 'core\core.a'; reason: File exists


    Multiple libraries were found for "ax12.h"
    Used: C:\Users\Che Edoga\Documents\Arduino\libraries\Bioloid
    Not used: C:\Users\Che Edoga\AppData\Local\Arduino15\packages\arbotix\har dware\avr\0.0.2\libraries\ArbotiX
    Not used: C:\Users\Che Edoga\AppData\Local\Arduino15\packages\arbotix\har dware\avr\0.0.2\libraries\ArbotiX
    Not used: C:\Users\Che Edoga\AppData\Local\Arduino15\packages\arbotix\har dware\avr\0.0.2\libraries\ArbotiX
    Not used: C:\Users\Che Edoga\AppData\Local\Arduino15\packages\arbotix\har dware\avr\0.0.2\libraries\ArbotiX
    exit status 1
    Error compiling for board Arbotix-M.


    This report would have more information with
    "Show verbose output during compilation"
    option enabled in File -> Preferences.

    Thanks for continuing to help.

    DB

  5. #15
    Join Date
    Dec 2007
    Location
    Whidbey Island, WA
    Posts
    1,718
    Images
    456
    Rep Power
    96

    Re: ArbotiX 1.6 Files / Libraries

    OK...success! The last bit was that I had the programmer plugged in backwards. :-( Thank you all so much! Now to run pypose and get this thing moving around!

    DB

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) difference of libraries between arbotix-0015 and robocontroller-0010
    By zhayantian in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 05-02-2014, 04:56 AM
  2. Question(s) Arbotix CAD files
    By kanuto in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 03-10-2014, 08:08 PM
  3. Arbotix CAD files
    By sarendt in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 10-24-2012, 02:31 PM
  4. MINI Robocontroller Libraries and Arduino 1.0
    By draikani in forum Software and Programming
    Replies: 3
    Last Post: 01-23-2012, 04:34 AM
  5. News/Announcement RX-28 and RX-64 Open-Source (Python) Libraries Available
    By hizook in forum Robotics General Discussion
    Replies: 1
    Last Post: 03-19-2010, 11:02 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •