Results 1 to 3 of 3

Thread: Arbotix-M Dimensions

  1. Arbotix-M Dimensions

    Dear All,
    While waiting for my Arbotix-M to arrive, I want to design the mechanical part to hold it.

    But I couldn't find its dimension anywhere, other than its size 61mm X 61mm.

    Can anybody point me to any document, or be kind enough to share these measurements;

    1. Outer dimension = 61mm X 61mm (correct?)
    2. Screw hole size = ?
    3. Screw hole location = ?

    Thanks!

    Arif

  2. #2

    Re: Arbotix-M Dimensions

    1)The ArbotiX-M is 61x61mm (the DC heck does overhang the PCB by ~1.5mm, so in a tight enclosure you'd need 61x62.5, or at least a cutout for the jack, plus any clearance for what you plug into it)

    2)The ArbotiX-M is deigned for M3 bolts (the actual hole size is ~3.3mm)

    3)The mounting holes are on a 52x52 mm square.

  3. Re: Arbotix-M Dimensions

    Fantastic! Thanks kgranat!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) MX-28, MX-64 and MX-106 Dual-Axis Joint Dimensions
    By vehemens in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 11-15-2015, 05:27 PM
  2. Question(s) ArbotiX with LabVIEW: Low-level ArbotiX Commands?
    By vogonpoet42 in forum Software and Programming
    Replies: 2
    Last Post: 03-01-2013, 11:25 AM
  3. Airsoft turret mechanism dimensions?
    By XZIVR in forum Mech Warfare
    Replies: 7
    Last Post: 04-10-2012, 01:23 AM
  4. mech airsoft gun dimensions + weight
    By societyofrobots in forum Mech Warfare
    Replies: 38
    Last Post: 07-11-2009, 02:55 AM
  5. Metal Servo Horn HMSH-02 Dimensions
    By Superlaxstar112 in forum Mechanics / Construction
    Replies: 0
    Last Post: 06-29-2008, 09:40 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •