Results 1 to 5 of 5

Thread: Is it easy to use MX-64/MX-28/AX-12A all together?

  1. Is it easy to use MX-64/MX-28/AX-12A all together?

    Building an arm using all three of these motors, is the integration/programming going to be a challenge using a servo not in the MX series>

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    285

    Re: Is it easy to use MX-64/MX-28/AX-12A all together?

    As long as you are using MX-28T and MX-64T at a baudrate of no more than 1Mbps, then you should have almost no problems with all of the servos chained together on a single dynamixel buss. Polling servo positions might give you a bit of trouble as the MX servos support sync_read and bulk_read functions that the AX servos do not, so just stick with individual read packets to get present position feedback from the servos and sync_write to send new goal positions to all servos at once. The AX servos and MX servos use different position ranges and resolutions (AX is 1024 ticks from ~30 to ~330 degrees with 180 located at top dead center; MX is 4096 ticks from 0 to 360 degrees with 180 located at top dead center), so any software should use degrees or radians in calculations/poses then convert each angle value to the proper goal position value for the given servo when building the sync_write packet to update the goal positions of all the servos simultaneously.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. Re: Is it easy to use MX-64/MX-28/AX-12A all together?

    Or you could avoid the limitations of using the AX-12 by using the MX-12.

  4. #4
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    285

    Re: Is it easy to use MX-64/MX-28/AX-12A all together?

    Only the MX-12W is commercially available, and it does not have the torque required for most joints. Modifying an MX-12W into an MX-12A by replacing much of the gearset is not something most beginners would be willing to try on their own when they can just buy the cheaper AX-12A that will work immediately.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  5. Re: Is it easy to use MX-64/MX-28/AX-12A all together?

    Quote Originally Posted by tician View Post
    Only the MX-12W is commercially available, and it does not have the torque required for most joints. Modifying an MX-12W into an MX-12A by replacing much of the gearset is not something most beginners would be willing to try on their own when they can just buy the cheaper AX-12A that will work immediately.
    Changing gears requires a screwdriver, cleanliness and some dexterity. Anyone working with these servos should know how to repair them.

    Using the MX-12 servo avoids the hardware and software limitations of the AX-12 servo mentioned earlier. Also the MX-12 magnetic position sensor will not wear out unlike that of the AX-12 potentiometer position sensor.

    Ultimately it's a trade space of time, money and skill which only memmerich can to do.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Alternate cheap/easy embedded platforms
    By TXBDan in forum Robot Computers
    Replies: 16
    Last Post: 02-03-2014, 09:54 AM
  2. cheap and easy mech or fighting robot
    By jiokl in forum Robotics General Discussion
    Replies: 1
    Last Post: 03-09-2012, 09:07 PM
  3. I-sobot + Arduino interfacing made easy
    By Nelsontheunholy in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 01-21-2010, 03:17 PM
  4. Easy Programing of servos and play back
    By hotrodled in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 01-30-2008, 03:18 PM
  5. Robot Tip: A Quick and Easy way to Mount Batteries
    By Matt in forum Robotics General Discussion
    Replies: 2
    Last Post: 12-21-2007, 06:53 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •