Results 1 to 4 of 4

Thread: PhantomX WidowX Payload Capacity

  1. #1

    PhantomX WidowX Payload Capacity

    Is there anyway to increase the payload capacity of the PhantomX WidowX? I.e is it possible to swap the Dynamixels with ones with higher torque or to potentially use the new pro series?

  2. #2

    Re: PhantomX WidowX Payload Capacity

    There are no other servos that exactly match the mounting holes of the MX-28.
    The only kinds of swappable Dynamixel servos I know about are:
    AX-12 can swap with AX-18
    MX-64 can swap with MX-106
    XH-430 can swap with XM-430

    That being said, once you get to the cost of the Pro servos, the additional cost of having some steel or aluminum plate water jet cut to match up the holes of the pro servos is comparatively small. Then again, if that's the kind of price range you're looking at, a small desktop factory robot arm from Kuka or ABB or whatever is probably a better option -- same price or cheaper, and comes fully production ready. (At least if you buy it used.)

  3. #3
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    79

    Re: PhantomX WidowX Payload Capacity

    Quote Originally Posted by jwatte View Post
    MX-64 can swap with MX-106
    You'll need wider C-brackets for the MX-106, unless you already use the brackets made for 106 with the additional spacers.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  4. #4

    Re: PhantomX WidowX Payload Capacity

    That's right -- I was thinking of the front/back hole patterns, which have the same spacing. The C brackets do not, as you say.
    (When I make my brackets, I try to avoid C / bent metal as much as possible, because I have a much easier time getting precision out of milled parts and drilled holes/screw connections.)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Does WidowX work with ROS arbotix_python?
    By RoBoCeRo in forum Interbotix Robotic Arms
    Replies: 1
    Last Post: 07-31-2015, 12:13 AM
  2. PhantomX Quadroped with heavier payload
    By jwatte in forum Humanoids, Walkers & Crawlers
    Replies: 7
    Last Post: 05-19-2015, 04:21 PM
  3. Bioloid Premium weight capacity
    By Franke in forum Humanoids, Walkers & Crawlers
    Replies: 18
    Last Post: 05-09-2013, 10:56 AM
  4. Question(s) Just Received WidowX Arm
    By mcintosh in forum Interbotix Robotic Arms
    Replies: 12
    Last Post: 12-20-2012, 12:46 AM
  5. Question(s) Recommendations for high capacity Lithium ion battery packs?
    By Pi Robot in forum Power
    Replies: 12
    Last Post: 09-20-2010, 02:06 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •