Results 1 to 3 of 3

Thread: Question(s): The RTeam Reference Design

  1. #1
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    50

    Question Question(s): The RTeam Reference Design

    For those not aware, RTeam is super awesome for making a full CAD model of a mech available at: https://github.com/bloftin/rbots/tree/master/Mech

    I'm going to adapt the forced-loader design from there. For the RTeam guys, I have a question: what size spiral cable wrap tubing did you find works best? I've looked over the BOM list a couple of times and I don't see it included. It seems like either 5/16" with about 0.03" wall, or 3/8" with 0.062" wall would be best. Is one better than the other? Thanks!

  2. #2

    Re: Question(s): The RTeam Reference Design

    The spiral cable wrap that we use has an I.D. of 1/4". The wall thickness does not seem to matter much except for flexibility. In order to make it so the BB's don't Jam or stick inside the tube, use a 1/4" dowel rod and wrap the spiral tubing tightly around it. Heat the spiral tubing with a heat gun until it starts to soften. Immediately cool the tubing under cold water and the spiral tube should hold it's shape. This method has worked the best so far.

  3. #3
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    50

    Re: Question(s): The RTeam Reference Design

    Thanks, Joey! That is a nice trick. I ended up finding some seemingly perfect tubing from this listing on ebay: http://www.ebay.com/itm/131973084196

    It's 5/16" OD (most of this tubing is advertised by OD), with unspecified wall thickness, but probably 0.03" or so. Though advertised as white, and shown as being translucent, I actually got black, which is what I really wanted anyways. I was able to fill a section of it with BBs and they move smoothly, so I will probably be able to skip the heating step. Next up is to build my prototype forced ammo loader!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. R+ Design
    By jwatte in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 01-02-2016, 08:07 PM
  2. RTEAM Robotics Club Mech Warfare 2015
    By artans in forum Mech Warfare
    Replies: 37
    Last Post: 06-22-2015, 11:27 AM
  3. (Hopefully) basic question on leg design.
    By escott76 in forum Humanoids, Walkers & Crawlers
    Replies: 16
    Last Post: 03-28-2013, 06:25 AM
  4. Project Xbee design help...
    By dannyboy in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 04-16-2010, 04:05 PM
  5. my beer-bot design
    By robot maker in forum Robotics General Discussion
    Replies: 12
    Last Post: 12-23-2008, 01:06 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •