Results 1 to 2 of 2

Thread: Turbo Fuse

  1. Question Turbo Fuse

    I just received the PhantomX robot arm and had a question about using Turbo Fuse for securing the screws. If I plan to build the arm but then intend to either mod it or take it apart, should I use the Turbo Fuse? Is that intended to be for permanent construction or will it be easy enough to take apart and put back together? I'd like to see how well it works initially and then be able to modify it as I need.

    Thanks!

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,266
    Images
    27
    Rep Power
    274

    Re: Turbo Fuse

    It is a ('blue') low strength anaerobic adhesive, so it easily removed with just a screwdriver or hex wrench and it is essential to keep the robot from shedding screws during usage. It provides just enough strength and resistance to keep the screws backing out on their own. It is the 'red' locktite you can find in big box stores that is a high/medium strength adhesive that requires significant heating to break the bonded surfaces loose.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project Mantis - Two Tonne Turbo Diesel Hexapod Walking Machine
    By mdenton in forum Project Showcase
    Replies: 22
    Last Post: 06-24-2013, 08:49 AM
  2. Bioloid Fuse
    By dantaylor129 in forum Robotics General Discussion
    Replies: 2
    Last Post: 11-06-2009, 11:06 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •