Page 2 of 2 FirstFirst 12
Results 11 to 19 of 19

Thread: Autocannon

  1. Re: Autocannon

    I sincerely look forward to seeing this completed, it would be a great addition to the "cheap weapons" category. Would you mind posting the hardware list for this, I'd love to experiment with this myself.
    Last edited by Thalvus; 11-17-2016 at 10:53 AM.
    Thalvus the ???
    the JgPz 38(t) Hetzer, my baby, my love, and my weapon of mass destruction

  2. Re: Autocannon

    I imagine you've already thought of this, but mounting the unit in the vertical configuration as a pitching machine does and then driving the motors at slightly different speeds you can achieve the same golf ball/airsoft hop-up effect by imparting a spin on the BB. Of course at the ranges this will likely be operating it might not matter, but still.

  3. #13
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    253
    Rep Power
    33

    Re: Autocannon

    Quote Originally Posted by fractura_laniatus View Post
    ...then driving the motors at slightly different speeds you can achieve the same golf ball/airsoft hop-up effect by imparting a spin on the BB.
    We have had similar discussions. We thought keep it mounted horizontally but drive the motors at different speeds and maybe we could spray the BBs.

    Haven't had any time to work on this further though since I posted the video. Way too much to do...

  4. #14
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    253
    Rep Power
    33

    Re: Autocannon

    Click image for larger version. 

Name:	RTeam Logo.jpg 
Views:	252 
Size:	11.1 KB 
ID:	6946
    http://rteamrobotics.weebly.com/

    Took a break from working on my Mech this weekend and trying to help out one of our club members get a light class Mech ready to compete. Working on a potential melee weapon. It consists of a sector gear driven by a XL320. Not quite as fast as I would like, but seems to be working. May have to try a lighter spring and see if I can speed it up a bit. I'll probably end up putting one on my Mech '99 as a close combat weapon as well.

    Click image for larger version. 

Name:	Metabot.jpg 
Views:	274 
Size:	65.8 KB 
ID:	6947


  5. #15
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    48

    Re: Autocannon

    Agh! I should have realized that the new score panels would make the auto-lance much more practical

  6. #16

    Re: Autocannon

    Gotta turn up the speed on my gait so I can run away and shoot from afar :-)

  7. #17
    Join Date
    May 2016
    Location
    White Plains, NY
    Posts
    124
    Images
    1
    Rep Power
    20

    Re: Autocannon

    Are we allowed to have a spatula to flip them onto their backs? Like a turtle?

  8. #18
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    283

    Re: Autocannon

    Quote Originally Posted by Brooks View Post
    Are we allowed to have a spatula to flip them onto their backs? Like a turtle?
    It is Mech Warfare, not plain robot combat. I could see a lance/sword being used to knock over and possibly invert an opponent, but not really a dedicated flipper/spatula mechanism.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  9. #19
    Join Date
    May 2016
    Location
    White Plains, NY
    Posts
    124
    Images
    1
    Rep Power
    20

    Re: Autocannon

    Quote Originally Posted by tician View Post
    I could see a lance/sword being used to knock over and possibly invert an opponent, but not really a dedicated flipper/spatula mechanism.
    Oh, crumbs! I had a mental picture of a mech with a kitchen spatula sticking out in front...

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •