Results 1 to 5 of 5

Thread: Capacitor for MX28?

  1. Capacitor for MX28?

    Hi
    I'm running a linear actuator and 2 mx28s from the same 12v power supply.
    The supply is rated for 10A, which should be fine I think.
    However, when the linear actuator starts or stops, the mx28s sometimes "reboot" (forget what they were doing). They work ok if I send them a new command, but otherwise lose torque.
    Should I put some kind of capacitor inline - if so, what size would you suggest?
    Or maybe some kind of battery arrangement?
    Thanks for any advice.
    Hugh

  2. #2

    Re: Capacitor for MX28?

    I would suggest a big capacitor (2200 uF ?) across the linear actuator. Perhaps also some clamping diodes.
    Capacitors across the MX-28s is also good. Somwhere between 470 uF and 1000 uF seems reasonable.
    However, this is just rule-of-thumb -- to really know what's going on, you need to hook up an oscilloscope both across the battery, across the linear actuator, and across the MX-28s.

  3. Re: Capacitor for MX28?

    Thanks - I'll give it a go. Sounds like i might need to work out an oscilloscope solution for myself too.

  4. #4

    Re: Capacitor for MX28?


  5. Re: Capacitor for MX28?

    I tried the capacitors, no difference.
    I swapped out the power supply for a better one, but only rated 2A, and it works fine. It appears to draw 0.7A while the actuator is running. So I'm thinking the power-brick style power supply is simply not up to rapid changes in current, even though it is rated 10A.
    As you say, an oscilloscope might tell a better story.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. MX28 temperature control
    By navidahmeduom in forum DYNAMIXEL & Robot Actuators
    Replies: 9
    Last Post: 05-19-2015, 06:53 AM
  2. Mx28 : Need help to control the goal position.
    By danyboy in forum DYNAMIXEL & Robot Actuators
    Replies: 11
    Last Post: 07-01-2013, 03:16 AM
  3. MX28 Setup with AX12 on the same USB2Dynamixel
    By dshinsel in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 01-13-2013, 11:59 AM
  4. Dynamixel MX28
    By Janis in forum DYNAMIXEL & Robot Actuators
    Replies: 9
    Last Post: 12-01-2012, 11:09 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •