Results 1 to 2 of 2

Thread: Two Position Servo?

  1. Two Position Servo?

    Hello,
    I am encountering a problem where an AX-18 servo bought as part of the set. One servo functions fine, but the other more uniquely: it will only go to two different positions, open and shut. I need a full range of motion. For example: when connecting solely to this servo with dynamanager, if the motor is at position 0, it will not move until I give it a position greater than the half way point, at which time the motor will move all the way open. Is this a setting? Has anyone heard of this before?
    Thanks, EricTheGreat

  2. #2

    Re: Two Position Servo?

    Sounds like the potentiometer is broken, perhaps?

    Try doing the firmware recovery. If it still has this problem, then some piece of hardware is broken, and the servo needs replacement (or at least service.)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Servo reading position and lock position CW
    By mkanon in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 03-30-2013, 04:10 PM
  2. Help with servo read position
    By starstorms in forum Software and Programming
    Replies: 1
    Last Post: 04-21-2012, 04:36 AM
  3. Interesting Hack servo v3.00 - Get full PID position and speed control from your hobby servo
    By Antonb in forum Mechanics / Construction
    Replies: 20
    Last Post: 06-27-2010, 10:24 AM
  4. Question(s) Arbotix problems with pose servo position
    By muc in forum Arbotix, Microcontrollers, Arduino
    Replies: 9
    Last Post: 02-21-2010, 06:11 PM
  5. PWM to Phidget Servo position function
    By Alex in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 08-13-2007, 05:02 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •