Results 1 to 9 of 9

Thread: How often to recharge LIPO battery?

  1. How often to recharge LIPO battery?

    Hello, is it a good idea to recharge LIPO battery every time after use? How often should we do it?

  2. #2

    Re: How often to recharge LIPO battery?

    A LiPo should not be discharged below 3.2V per cell.
    It also has a slow self-discharge, so if you're not going to use it for many months, giving it a charge so you know it won't go below 3.2V is helpful.
    Charging all the way to full (4.2V / cell and only a small current remaining) will wear the oxide in the cell, though, and thus "consume life" of the cell. Charging it up to a lower voltage will damage it less.

    Thus, a good idea might be to charge to 3.9V or 4.0V per cell, use a trickle charge like 0.2C, and cut off the charging once it gets there. This will pad against self-loss, and also make sure that the battery is at least 70% or so ready to be used if you need it immediately, yet not wear it out too much. (This is what I generally do.)

    Note that you'll need to use a charger that lets you set the voltage. Personally, I use a high quality benchtop power supply, and charge the full stack (without worrying about balance.) I set the current limit to something small, and then keep an eye on it, and when the battery draws less than the current limit, at the target voltage, I call it done.
    Once I want to charge it full, I use a balance charger to make sure the cells are in "harmony," but you really don't need to do that every time you charge.

  3. #3
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    788
    Images
    276
    Rep Power
    74

    Re: How often to recharge LIPO battery?

    Some chargers have an option called "Storage charge". About 50% capacity is ideal if you are not going to use it immediately.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  4. Re: How often to recharge LIPO battery?

    Thanks jwatte and Zenta. I bought a SKYRC iMax B6AC version 2 AC/DC Dual Power Professional Balance Charger/Discharger. Have not used it before. Is there a step-by-step guide on how to do what you suggested using this device?

  5. #5
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    788
    Images
    276
    Rep Power
    74

    Re: How often to recharge LIPO battery?

    I did a fast search on you charger and found that it has the option for "Storage charge" :
    "Store" setting will charge the battery at approximately a 50% charge for long term storage. This prolongs the useful life of the battery pack.
    I recommend reading the manual.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  6. Re: How often to recharge LIPO battery?

    Quote Originally Posted by Zenta View Post
    Some chargers have an option called "Storage charge". About 50% capacity is ideal if you are not going to use it immediately.
    Thanks. Assuming that I do a 50% storage charge now and when I need to use the battery again, should I recharge it more?

  7. #7

    Re: How often to recharge LIPO battery?

    Yes, that would be optimal.
    If you know that you will use the battery within a week or two, though, just charge it full right away.

  8. #8
    Join Date
    Apr 2013
    Location
    Boston, MA
    Posts
    260
    Images
    11
    Rep Power
    23

    Re: How often to recharge LIPO battery?

    I've had a couple LiPo packs sitting for a couple years... in terms of safety, what should I do with them? attempt to charge? dispose somehow?

  9. #9

    Re: How often to recharge LIPO battery?

    Put a voltage meter to them. If the voltage is 3.0 volts per cell or better, you should be able to charge them and use them. If it's much less than that, it's probably better to throw them out.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. lipo battery for irobot
    By hazaza in forum Power
    Replies: 5
    Last Post: 04-18-2013, 08:00 PM
  2. Question(s) Max amp load on LiPo battery
    By alonso in forum Power
    Replies: 7
    Last Post: 04-06-2013, 01:42 AM
  3. Question(s) 4S 14.8v lipo battery is charging to 16.5v??
    By alonso in forum Power
    Replies: 2
    Last Post: 10-14-2012, 11:23 PM
  4. Question(s) Monitoring LiPo battery while it's in use.
    By Stobs in forum Power
    Replies: 4
    Last Post: 10-04-2011, 10:01 AM
  5. Question(s) LiPo Battery cut off safety?
    By Pinter75 in forum Power
    Replies: 11
    Last Post: 03-15-2009, 04:52 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •