Results 1 to 5 of 5

Thread: Mechanical drawing of the Double Eagle AEG?

  1. #1

    Mechanical drawing of the Double Eagle AEG?

    Does anyone have a good mechanical drawing of the Double Eagle AEG?

  2. #2
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    253
    Rep Power
    28

    Re: Mechanical drawing of the Double Eagle AEG?

    I have a model of an AEG gearbox I can post for you. It's not specifically Double Eagle but all the AEG gearboxes seem to be very similar with just minor differences between them.

    Its based of me just measuring one with a caliper, fitting it to my 3D printed parts, and re-tweaking the model.... so its not 100% accurate but good enough.

    I have it as a .prt file, what format do you need? I can easily convert it to one of the common formats (igs, stp, stl) if needed.

    I'll try to post it tonight or tomorrow evening.

  3. #3

    Re: Mechanical drawing of the Double Eagle AEG?

    stp would be okay, but best would be flat drawing! (dxf, dwg, etc.)
    I used to have one, based on a photo I took and measured on, but I have misplaced it.
    (That's what I used to build the bundle of robot parts which makes for a well-tested hop-up/feed/mount for these.)

    (Edit: I found it!)



    Dimensions are in mm, "T" means depth of the area with the hole, presumably symmetrically distributed across the center plane.
    Holes are, IIRC, M3 for two of them and M4 for the rearmost one.
    Last edited by jwatte; 02-01-2017 at 01:52 PM.

  4. #4
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    253
    Rep Power
    28

    Re: Mechanical drawing of the Double Eagle AEG?


  5. #5

    Re: Mechanical drawing of the Double Eagle AEG?

    Nice!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Double Eagle gearbox questions
    By jwatte in forum Mech Warfare
    Replies: 3
    Last Post: 12-15-2014, 10:30 AM
  2. Just For Fun A Humaniod Robot drawing for ideas ......
    By sweldon in forum Off Topic
    Replies: 3
    Last Post: 03-17-2013, 02:54 PM
  3. Project Line Drawing Robot
    By arcadefreaque in forum Projects For Request and/or Sale
    Replies: 9
    Last Post: 08-05-2011, 02:53 PM
  4. AX-18F = AX-12+ with a double torque. Crazy idea?
    By RobotAtlas in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 06-13-2010, 07:34 PM
  5. Mechanical Engineer
    By valleycycles in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 01-13-2009, 06:45 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •