Page 2 of 3 FirstFirst 123 LastLast
Results 11 to 20 of 21

Thread: Falling-Up Robot Project

  1. #11
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    26

    Re: Falling-Up Robot Project

    Sweet project! I love how massively tall this robot stands. Might be pretty crazy to scale it wider and make something like wall dividers that you or two people could push around.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  2. Re: Falling-Up Robot Project

    Quote Originally Posted by tician View Post
    NEMA sized hybrid stepper motors may be a bit heavier and lower power, but they are inexpensive, accurate, and can use small, inexpensive micro-stepping drivers for accurate position control without any gearing. The extra weight of the stepper motor is coaxial with the wheel, so has very little effect on the pendulum's moment of inertia and ultimate payload. If you absolutely do not want any gearing, you are pretty much stuck with stepper motors. There are low backlash gear boxes and/or roller chain / timing belt setups that would enable hobby BLDC motors to provide similar performance to a heavier stepper motor using direct drive, but they can be expensive and/or bulky.
    Very low backlash gearmotors are available, but are very expensive, upwards of $200 USD depending on desired specs. And the torque at low speed is still low compared to steppers.

    The NEMA23 3A stepper motors used on the Falling-Up Robot have a max holding torque of 270 oz-inches without a gearbox. So there's no issue with wearing out gears. The torque combined with zero backlash results in very nice stand-still performance. For high rate corrections, the steppers are very responsive:

    https://forum.pjrc.com/threads/41442...l=1#post132162

    For those who attempt stepper motors, driving them is not as straightforward as a DC motor with PWM control. Also, steppers induce more mechanical vibration that DC gearmotors. Microstepping is necessary and I recommend stepper drivers with sinusoidal current control. Filtering the accel & gyro measurements is also a must.

  3. Re: Falling-Up Robot Project

    Quote Originally Posted by r3n33 View Post
    I love how massively tall this robot stands. Might be pretty crazy to scale it wider and make something like wall dividers that you or two people could push around.
    I didn't have the heart to cut the 6 foot long aluminum extrusions. It turned out that It makes for a very interactive robot because it stands with you. And the main microcontroller board is at desk level, so it's convenient to work with, without taking precious space from my desk.
    Extrusions are great for making very light and stiff robot frames. It's easy to add parts without having to disassemble your project. They're like legos for adults.

  4. #14

    Re: Falling-Up Robot Project

    It makes for a very interactive robot because it stands with you
    That's a great observation!

  5. Re: Falling-Up Robot Project

    Okay, I got the XBEE communication working with the Teensy 3.6 mcu, and able to send motion commands to the Falling-Up Robot. Able to yaw and translate the 6-foot robot while maintaining tilt stability. It's no longer tethered to the USB port and the power supply unit. See latest video below. Recommend headphones.

    https://www.youtube.com/watch?v=QHb9eYAyGJc

  6. #16

    Re: Falling-Up Robot Project

    Nice wood floors. And kid play capsule :-)

    That bot has to be over 2 meters tall now? It seems to reach almost to the ceiling.

  7. Re: Falling-Up Robot Project

    Quote Originally Posted by jwatte View Post
    Nice wood floors. And kid play capsule :-)

    That bot has to be over 2 meters tall now? It seems to reach almost to the ceiling.
    It's two meters tall. Didn't have the heart to cut the aluminum extrusions. I figured, why do bots need to be toy-sized, why not people sized?

  8. #18

    Re: Falling-Up Robot Project

    why do bots need to be toy-sized, why not people sized
    The first time it knocks a vase off a mantlepiece, you'll have your answer :-)

    I kind-of agree, though. While I'm building a 2-foot walking robot, I dream of building a 4-meter walking robot ...

  9. #19
    Join Date
    May 2016
    Location
    White Plains, NY
    Posts
    113
    Images
    1
    Rep Power
    6

    Re: Falling-Up Robot Project

    Quote Originally Posted by jwatte View Post
    While I'm building a 2-foot walking robot, I dream of building a 4-meter walking robot ...

  10. Re: Falling-Up Robot Project

    A bit stuck with Integral Windup in the PID control system. It's especially a problem if the robot is lifted or gets stuck in a corner. The integral error blows up. I want to implement the Back-Calculation method for alleviating Windup, but I need more information on this. Any recommendations on a good Feedback Control Systems book for robotics?

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX ROS Robot Project
    By ezex in forum Humanoids, Walkers & Crawlers
    Replies: 33
    Last Post: 04-19-2014, 11:02 AM
  2. Contest Entry The Pi Robot Project
    By Pi Robot in forum Project Showcase
    Replies: 18
    Last Post: 01-24-2011, 09:19 AM
  3. Question(s) has any build the oap robot project
    By robot maker in forum Robotics General Discussion
    Replies: 23
    Last Post: 08-27-2008, 10:47 PM
  4. My Robot Project
    By Jeff Terrell in forum Rovers
    Replies: 26
    Last Post: 08-07-2008, 04:02 PM
  5. My Robot Project
    By Jeff Terrell in forum Robotics General Discussion
    Replies: 22
    Last Post: 01-29-2007, 10:31 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •