Page 1 of 3 123 LastLast
Results 1 to 10 of 21

Thread: Falling-Up Robot Project

  1. Falling-Up Robot Project

    I'm developing the Falling-Up Robot, a very tall balancing inverted pendulum bot, using the Teensy 3.6 microcontroller with Arduino IDE 1.6.12. I want to practice feedback control systems with this robot. I want to keep it from falling over while roaming autonomously and interacting with its environment. I'm building this in stages. So far, the brain and chassis is in place, and the basic balancing control system is in place. Here's the first video.



    I used stepper motors to take advantage of high torque at low RPM and zero backlash (or zero freeplay). Dealing with the high mechanical vibration was an issue, but was solved with analog filters in the IMU and an Extended Kalman Filter in software.

    More details here:
    https://forum.pjrc.com/threads/41442...for-Teensy-3-6

  2. #2

    Re: Falling-Up Robot Project

    That's quite the tall robot! I like it.

    When it comes to "zero" backlash: Did you compare direct-drive brushless DC motors with stepper motors?

  3. Re: Falling-Up Robot Project

    Quote Originally Posted by jwatte View Post
    When it comes to "zero" backlash: Did you compare direct-drive brushless DC motors with stepper motors?
    Direct drive motors would do the job too, but are pricey. The power savings is attractive. Steppers are power hogs but about the same price as a good hobby gear motor. I did get quotes on near-zero backlash gear motors, but were too expensive ($200+).

  4. #4

    Re: Falling-Up Robot Project

    Got it! As long as you use tethered power, or have batteries to spare, steppers are a fine solution.
    If you want this to rove autonomously for a longer while, then the cost of extra batteries versus the cost of motors becomes an equation to solve.

    Good luck with the project! I would love to see another post when you get more bits going.

  5. #5
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,227
    Images
    27
    Rep Power
    270

    Re: Falling-Up Robot Project

    Eh? I'm rather curious as to how steppers are classified as power hogs, but BLDCs are not.

    Stepper motors and BLDCs are both permanent magnet synchronous motors. There are many many configurations including 2-phase, 4-phase, 5-phase, etc. stepper motors, and 3-phase, 2-phase, etc. BLDCs. The only real differences between a stepper motor and a BLDC are determined by the intended use via: 1) the turn count of the windings and 2) the apparent number of poles on the rotor and stator. Steppers are almost universally wound with high turn counts and many poles for lower speed and very high torque at low current - which greatly limits maximum power in a given size/package - while BLDCs tend to be wound with low turn counts and fewer poles for high speed and decent torque at very high current for moar powah.





    Also kinda curious why the Clockwork Orange rendition of Henry Purcell's "Funeral March for Queen Mary" was used in that video.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  6. #6

    Re: Falling-Up Robot Project

    I'm rather curious as to how steppers are classified as power hogs, but BLDCs are not.
    I think it has more to do with what kind of packaging is easily available.
    Steppers almost universally come in large, clunky steel casings, which are perfect for rigid floor-mounted machines, but bad for mobility.
    BLDCs have been optimized (especially by the RC and Quadcopter folks) to be much more light-weight for the power.
    Thus, lower inertia, faster response, and less load to lug around.

  7. Re: Falling-Up Robot Project

    Quote Originally Posted by tician View Post
    Eh? I'm rather curious as to how steppers are classified as power hogs, but BLDCs are not.
    I have not used brushless DC motors for these balancing robots. On the other hand, I've used standard brushed gear motors along with steppers. Most of the time, the robot is just standing still making small corrections. The DC motor hardly consumes power, but the backlash and low torque at low RPM makes the stand-still response not very steady. In contrast, the stepper motor pair consumes about 0.6 to 0.7 amps even at zero RPM according to my desktop power supply. But the torque is very high, which is highly desirable. Along with zero backlash, I get very stable stand-still response. I think the best solution would be a direct drive motor as @jwatte suggested, but that route is pricey. For now, recharging the Lipo's for the steppers is a workable solution.

    Quote Originally Posted by tician View Post
    Also kinda curious why the Clockwork Orange rendition of Henry Purcell's "Funeral March for Queen Mary" was used in that video.
    It has a thought-provoking quality to it, plus the electronic instrumentation goes hand-in-hand with robotics.

  8. #8
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,227
    Images
    27
    Rep Power
    270

    Re: Falling-Up Robot Project

    Quote Originally Posted by jwatte View Post
    I think it has more to do with what kind of packaging is easily available.
    Steppers almost universally come in large, clunky steel casings, which are perfect for rigid floor-mounted machines, but bad for mobility.
    BLDCs have been optimized (especially by the RC and Quadcopter folks) to be much more light-weight for the power.
    Thus, lower inertia, faster response, and less load to lug around.
    But power and torque are not the same thing; torque is merely one component of power along with speed. Traction motors require much more torque than needed to swing any propeller. You can get ridiculous power 'ratings' from lightweight R/C plane and multi-rotor motors because they run at incredibly high speed and low torque, which is inadequate for direct-drive traction motors in anything heavier than a mouse-sized speed-run maze-solving bot. Even the giant melon class (>50mm stator; ~0.8kg) out-runners with Kv in the <800 RPM/V range require some amount of gearing in traction applications with a vehicle more than a few times the weight of the motor unless you plan on it constantly pulling >20A per phase. Steppers tend to have Kv in the <50RPM/V range, so they always provide much more torque for a given current with lower overall power ratings (even rather large NEMA34 steppers are almost always rated below 10A continuous).


    Compare and contrast:

    • Probotix HT23-180-8 stepper wired in bipolar parallel (~$40)
      • Current(max): ~2.5[A]/phase
      • Torque at 2.5A/phase: ~13.35[kg-cm]



    • Turnigy Aerostar 6374-149 outrunner (~$80)
      • Current(max): ~70[A]/phase
      • Torque at 2.5A/phase: ~3.27[kg-cm]



    Again, steppers and BLDC are both permanent magnet synchronous motors but with designs suited for different uses. Steppers are suited for lower speed, direct drive traction/position control applications because of their high torque and high apparent pole count (one full electronic commutation cycle results in a very small mechanical rotation of the rotor). Hobby BLDC without gearing are suited for high speed, low torque speed control applications like propellers, turbines, and electric chainsaws (one full electronic commutation cycle results in a rather large mechanical rotation of the rotor). If you add sufficient gearing, BLDCs work wonderfully in traction applications and high-torque power tools but that gearing is absolutely required unless you want to deal with very high continuous currents. There are low backlash gear and belt systems, but they can get a bit expensive unless you have access to a machine shop to make your own.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  9. #9

    Re: Falling-Up Robot Project

    There are brushless gimbal outrunners that optimize more for torque and less for high speed.
    As you say, "melon class": https://hobbyking.com/en_us/turnigy-...otor-bldc.html
    Cheaper options: https://hobbyking.com/en_us/turnigy-...otor-bldc.html etc.
    Aaaanyway. It's fun to see such a big balancing robot with steppers!

  10. #10
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,227
    Images
    27
    Rep Power
    270

    Re: Falling-Up Robot Project

    Indeed, but they offer the same performance (angular resolution of maybe 7.5 degrees per step) as cheap pancake stepper motors while requiring 3-phase motor controllers that need to be programmed for position control instead of speed control. Very few 3-phase hobby controllers use vector control (field oriented control) or anything similar to micro-stepping which would be necessary for such a low resolution motor to direct drive a wheel on an inverted pendulum bot. And that smaller, cheaper one would never have enough power to control something as large as Falling-Up (12V max with 13Ohm phase resistance).

    NEMA sized hybrid stepper motors may be a bit heavier and lower power, but they are inexpensive, accurate, and can use small, inexpensive micro-stepping drivers for accurate position control without any gearing. The extra weight of the stepper motor is coaxial with the wheel, so has very little effect on the pendulum's moment of inertia and ultimate payload. If you absolutely do not want any gearing, you are pretty much stuck with stepper motors. There are low backlash gear boxes and/or roller chain / timing belt setups that would enable hobby BLDC motors to provide similar performance to a heavier stepper motor using direct drive, but they can be expensive and/or bulky.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX ROS Robot Project
    By ezex in forum Humanoids, Walkers & Crawlers
    Replies: 33
    Last Post: 04-19-2014, 11:02 AM
  2. Contest Entry The Pi Robot Project
    By Pi Robot in forum Project Showcase
    Replies: 18
    Last Post: 01-24-2011, 09:19 AM
  3. Question(s) has any build the oap robot project
    By robot maker in forum Robotics General Discussion
    Replies: 23
    Last Post: 08-27-2008, 10:47 PM
  4. My Robot Project
    By Jeff Terrell in forum Rovers
    Replies: 26
    Last Post: 08-07-2008, 04:02 PM
  5. My Robot Project
    By Jeff Terrell in forum Robotics General Discussion
    Replies: 22
    Last Post: 01-29-2007, 10:31 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •