Results 1 to 3 of 3

Thread: OpenCN904 to R+motion connection problems

  1. #1
    Join Date
    Oct 2013
    Location
    Los Angeles, CA
    Posts
    3
    Rep Power
    0

    OpenCN904 to R+motion connection problems

    I am trying to use the robotics software suite for the first time. I have some dynamixel xl320 hooked to a OpenCM9.04...
    no problems using the OpenCM IDE, but cant get the board to connect to the PC software such as R+ Motion... It tries but fails.
    Is this done through the micro USB port on the board? do I need a programmer module for this to work? Is there any code that I need to load from the IDE to get it to communicate with the software?

    I have a USB2Dynamixel adapter and have the USB Downloader LN-101 on the way...

    Still not sure what is the correct way to get the hardware and software to talk...

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,291
    Images
    27
    Rep Power
    276

    Re: OpenCN904 to R+motion connection problems

    You have to connect it to the PC with the USB cable and run a controller firmware update using RoboPlus Manager to erase any existing sketch from the OpenCM IDE and replace it with the Robotis RoboPlus firmware.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  3. #3
    Join Date
    Oct 2013
    Location
    Los Angeles, CA
    Posts
    3
    Rep Power
    0

    Re: OpenCN904 to R+motion connection problems

    THANK YOU!!! The firmware was way out of date!!!
    Now the software connects but the servos still are not being seen... Just before I posted this, I finished updating the firmware on the 3 XL320s they are all up to date, connected in chain to the board and have two batteries attached...
    the R+Motion software just shows ? next to the servos and says joint count:0
    Click image for larger version. 

Name:	Capture.jpg 
Views:	173 
Size:	86.7 KB 
ID:	6861

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Help Shield Connection
    By Jen17 in forum Software and Programming
    Replies: 0
    Last Post: 04-30-2014, 01:48 AM
  2. Bioloid Wireless connection problems
    By V4mp in forum Humanoids, Walkers & Crawlers
    Replies: 23
    Last Post: 01-29-2012, 11:21 PM
  3. Maxstream XBee connection problems
    By timothyahong in forum Arbotix, Microcontrollers, Arduino
    Replies: 5
    Last Post: 05-11-2011, 07:07 PM
  4. Question(s) Motion sequencing in RoboPlus Motion?
    By jarred in forum Software and Programming
    Replies: 4
    Last Post: 05-07-2010, 09:54 AM
  5. Bioloid ZIG-100 connection issue
    By kamondelious in forum Humanoids, Walkers & Crawlers
    Replies: 10
    Last Post: 10-12-2008, 01:24 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •