Hi all,
I'd like to introduce Quadbot 17, a quadruped robot born out of a learning exercise in Autodesk Fusion 360. The robot currently only exists as a CAD model, but with any luck it will become a reality soon!
It will use AX-12A Dynamixel servos (might be upgraded to the more powerful AX-18A). The legs currently have 20 DOF and there are an additional 2 DOF for the body. Servos and brackets are from the Robotis range, with some replaced by their metal counterparts available from Trossen Robotics. They will be painted to match the colour theme. The rest of the parts will be mostly 3D printed where appropriate. The main framework of printed parts forming the body will be sandwiched between 1.6 mm thick custom (laser-cut?) aluminium plates.
The novel aspects of this quadruped are its articulated legs, which have higher DOF than usually found on small quadrupeds, and its articulated "spine", which will help it in navigating uneven terrain.
This robot shares many ideas and knowledge gained from my other Dynamixel-based robot, the ROSoloid. Whether or not it gets integrated with ROS and the custom GUI remains to be seen. At the very least, the Raspberry Pi will run the kinematics and walking gait code.
One main thing I felt the ROSoloid humanoid robot was missing was an advanced sensory system. The advantage of the quadruped is its capability to carry heavier loads and provide a stable platform for sensors, hence the idea to add a Kinect! Its size seems to be perfectly fitting with the rest of the profile.
The build progress of this robot can be followed here.
Comments, suggestions and feedback are always welcome!
Bookmarks