Very nice! (Despite the black-on-black color scheme ;-)
You'll probably want to turn that back once you put real load on the robot. The load (and mass) of the full system will significantly change the dynamics parameters needed.The servos initially juddered a lot with default AX-12 settings, particularly the ankle and knee.
One way of somewhat emulating the real load in a test rig might be to add torsion springs on the joints. The benefit of that would be that you can then turn the spring direction around and make them counteract gravity when you build the full robot, to take some load off the servos.
This is the point at which I usually recommend people to buy a Saleae Logic device :-)I occasionally lose leg control and I'm not sure yet if it's serial failure or something else.
You can tie it into a number of points in your chain (early serial output, other end of serial wire, DXL bus TTL line, various test pins, etc) and get a comprehensive look at where the data goes and what it looks like; where delays are; etc.
Bookmarks